SNOAA68 June 2021 LMG3410R050 , LMG3410R070 , LMG3410R150 , LMG3411R050 , LMG3411R070 , LMG3411R150 , LMG3422R030 , LMG3422R050 , LMG3425R030 , LMG3425R050 , LMG3522R030-Q1 , LMG3526R030
All trademarks are the property of their respective owners.
For a new technology to be successful, it must be reliable in the customer application. Silicon power transistors are now regarded as reliable, but this was not always the case. Confidence in their reliability developed with longstanding experience, resulting in a well-accepted qualification methodology whereby reliability and quality are certified by running standardized tests and using reliability models for lifetime calculations. These tests were developed to accelerate failure mechanisms, with reliability engineering conducted to achieve the desired lifetime.
GaN transistors have now been known for 28 years(1). RF GaN FETs are now widely deployed in cellular base stations. Power GaN FETs are more recent, with development efforts starting in the early twenty first century. The power GaN industry does not have the luxury of time, so has invested considerable effort to accelerate reliability development. As a result, power GaN FETs are now considered reliable and are being deployed in both commercial and automotive products.
A key criterion is the reliable product operation for a broad range of customer applications under both normal and extreme use conditions. The traditional silicon approach, does not adequately address the switching conditions of power management, so we have built upon it. Our approach is shown in Figure 1-1, and consists of GaN-specific methodology to address switching reliability, conduct test, address failure modes, extrapolate lifetime, and ensure operation under extreme conditions such as lightning surge and short circuit.
The methodologies of Figure 1-1 result from several other aspects important for technology maturity. First is the formation of the JEDEC JC-70 committee on Wide Bandgap Power Electronic Conversion Semiconductors, with three GaN-specific guidelines already released: JEP173, JEP180, and JEP182. Second is the creation of a body of literature on failure mechanisms and their acceleration. Third is the thought leadership around a common approach for application reliability, a challenging topic. TI has played a leadership role in all these aspects. As a result, TI GaN products incorporate a well-developed methodology to validate and assure the reliability of GaN under all conditions of operation.
The objective of this white paper is to describe the progress and methodology by which TI GaN product reliability is assured and to show results that demonstrate lifetime reliability in application.
The qualification standards in use for silicon were first published in the 1990’s. The popular JEDEC JESD47 standard(2), “Stress-Test-Driven Qualification of Integrated Circuits” was first published in July 1995 and the Automotive Electronics Council (AEC) Q100(3) was first published in June 1994. These standards specify many tests which may be classified into three categories: device, electrostatic discharge (ESD), and package. At the time, memory and logic were the predominant applications, and the accelerated bias tests were intended to achieve an electric-field equivalent lifetime. The switching transitions of power management applications were not specifically considered.
Traditional device qualification is run by using a 1000h test at a junction temperature of 125ºC or higher at the maximum operating voltage. Running at 125ºC is equivalent to about nine years of use at Tj = 55ºC using an assumed activation energy of 0.7 eV.
Many of the tests also require a large number of parts to obtain defectivity and failure in time (FIT) statistics. For further background on traditional silicon qualification, see references 4 and 5.
Although JEDEC specifies the need for dynamic testing, conditions are not prescribed due to the ever-evolving applications and material sets in our industry(6). The field of power conversion illustrates the difficulties. There are many different topologies and numerous components with which the GaN FET interacts. Determining the lifetime of a GaN FET in a power converter is challenging for the following reasons. First, running acceleration studies could cause many non-GaN failures. Second, the applicability to different topologies would not be clear. Third, the energy usage of running the large number of power converters needed is large. It has therefore not been straightforward to assure product-level reliability in a broad sense. As a result, traditional reliability testing has not covered the switching conditions of power management.
The need for GaN-specific reliability validation arose because traditional silicon qualification methodology was not fully addressing application reliability for GaN products. During the early days, we observed that hard-switched transitions were causing overheating and occasional hard-failure. This finding is important because a broad class of power conversion applications are hard-switched. We developed a comprehensive methodology for qualifying the reliability of GaN products, described in references 4 and 5. The papers describe a common approach of validating the application reliability of GaN FETs for a broad class of applications.
The common approach is enabled by use of the switching locus curve to represent the type of switching stress applied to the device, and thereby the failure mechanism exercised. The switching locus curve is the trajectory of the iD-vDS waveform during a switching cycle(7). A test vehicle circuit with a hard-switching locus will therefore apply relevant stress for hard-switching applications(7).
Our test vehicle circuit shown in Figure 2-1 and described in references 4 and 5, is a boost converter stage with the output tied to the input to conserve energy. It is a similar circuit to the double pulse tester (DPT) with a different control. We use it in continuous-pulse mode for providing accelerated hard-switching stress per JEP182(8). A highly-reliable diode is used for the high-side device, eliminating high-side drive complexity. Its simplicity minimizes system-related failures, enabling accelerated testing for the desired failure mechanism. It is also designed to measure dynamic RDS(ON) per JEP173(9).
Traditional silicon qualification testing alone is not a guarantee for reliable application performance because it does not include hard-switching transitions, nor does it test for dynamic RDS(ON). Both aspects are very important for the proper operation of all devices in hard-switching applications. We have seen that GaN devices from processes that pass traditional silicon qualification can still overheat and show a decrease in efficiency when run in a in a hard-switched application. However, parts run reliably if the process passes traditional qualification testing plus hard-switching reliability testing(10).
It is often asked whether a device that is robust to hard-switching is also robust for soft-switching applications. This is reasonable thinking because hard-switching creates more hot electrons, which can increase electron trapping and result in higher dynamic RDS(ON)(11). It was previously shown(10) that hard-switching is the more stressful case for TI GaN devices. However, there have been recent literature reports(12) that soft-switching can cause higher dynamic RDS(ON) for some types of devices. Our stress testing confirms that TI GaN devices are reliable for both hard and soft-switching applications and confirms that soft-switching does not cause higher dynamic RDS(ON) for GaN technology in general.