SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The CC3x20, CC3x35, and CC3x30 devices are part of the SimpleLink™ microcontroller (MCU) platform which consists of Wi-Fi®, Bluetooth® low energy, Sub-1 GHz and host MCUs, which all share a common, easy-to-use development environment with a single core software development kit (SDK) and rich tool set. A one-time integration of the SimpleLink™ platform enables you to add any combination of the portfolio’s devices into your design, allowing 100 percent code reuse when your design requirements change. For more information, visit www.ti.com/simplelink.
The SimpleLink™ Wi-Fi®Internet-on-a chip™ family of devices from Texas Instruments™ provides a suite of integrated protocols for Wi-Fi® and Internet connectivity to dramatically simplify the implementation of Internet-enabled devices and applications.
This document provides software (SW) programmers with all of the required knowledge for working with the networking subsystem of the SimpleLink™ Wi-Fi® devices. This guide provides basic guidelines for writing robust, optimized networking host applications, and describes the capabilities of the networking subsystem. The guide contains some example code snapshots to give users an idea of how to work with the host driver. More comprehensive code examples can be found in the formal software development kit (SDK). This guide does not provide a detailed description of the host driver APIs.
SimpleLink, Internet-on-a chip, Texas Instruments, SmartConfig, and are trademarks of Texas Instruments Incorporated.
Wi-Fi and Wi-Fi Direct are registered trademarks of Wi-Fi Alliance.
Bluetooth is a registered trademark of Bluetooth SIG, Inc.
Arm and Cortex are registered trademarks of Arm Limited.
Google is a registered trademark of Google, Inc.
All other trademarks are the property of their respective owners.
This chapter gives a brief introduction to the networking subsystem, lists the key features of the device, and provides an overview of the host driver.
The SimpleLink™ Wi-Fi® family of devices consist on two types of devices: wireless MCU devices with a built-in network processor, and network processor standalone devices.
The SimpleLink™ Wi-Fi® CC31xx wireless network processor allows the connection of any low-cost, low-power microcontroller (MCU) to the Internet of Things (IoT), using standard communication interfaces such as SPI or UART. The scope of this document covers the following part numbers belonging to this type: CC3120, CC3130, and CC3135.
The SimpleLink™ Wi-Fi® CC32xx is a wireless MCU with an integrated high-performance Arm®Cortex®-M4 MCU, built-in Wi-Fi®, and a networking subsystem, allowing developers to write an entire application with a single-chip solution. The scope of this document covers the following part numbers belonging to this type: CC3220R, CC3220S, CC3220SF, CC3235S, CC3235SF, CC3230S, and CC3230SF.
The SimpleLink™ Wi-Fi®Internet-on-a chip™ family of devices introduces some advanced features and capabilities that further simplify connectivity of devices to the Internet:
Table 2-1 lists the key features of the SimpleLink™ Wi-Fi® device family.
Feature | Description | CC3120/CC3220 | CC3135/CC3235 | CC3130/CC3230 |
---|---|---|---|---|
Wi-Fi standards | 802.11b/g/n station | + | + | + |
802.11b/g access point with support for up to four stations | + | + | + | |
Wi-Fi Direct client / group owner | + | + | + | |
802.11a | + | |||
WFA IOT Low Power | + | + | ||
Wi-Fi channels | 1–13 | + | + | + |
36,40,44,48,52,56,60,64,100,104,108,112,116,120,124,128,132,136,140,149,153,157,161,165 | + | |||
Personal and Enterprise Wi-Fi security | WEP, WPA/WPA2 PSK | + | + | + |
WPA2+PMF, WPA3 | + | + | ||
WPA2 Enterprise (802.1x) | + | + | + | |
Wi-Fi provisioning | SmartConfig™ technology | + | + | + |
Wi-Fi Protected Setup (WPS2) | + | + | + | |
Access point mode with internal HTTP web server | + | + | + | |
IP protocols | IPv4/IPv6 | + | + | + |
IP addressing | Static IP, LLA, DHCPv4, DHCPv6 with DAD | + | + | + |
Cross layer | ARP, ICMPv4, IGMP, ICMPv6, MLD, NDP | + | + | + |
Transport | UDP, TCP | + | + | + |
SSLv3.0/TLSv1.0/TLSv1.1/TLSv1.2 | 6 | 16 | 16 | |
RAW | + | + | + | |
Network applications and utilities | Ping | + | + | + |
HTTP/HTTPS web server (including dynamic user call backs and RESTful API support) | + | + | + | |
mDNS | + | + | + | |
DNS-SD | + | + | + | |
DHCP server | + | + | + | |
OCSP TLS extension | + | + | ||
Host interface | UART/SPI | + | + | + |
Security | Secure key storage | + | + | + |
Trusted root-certificate catalog | + | + | + | |
TI root-of-trust public key | + | + | + | |
File system security | + | + | + | |
Secure boot | + | + | + | |
Secure content delivery | + | + | + | |
Initial secure programming | + | + | + | |
Debug security | + | + | + | |
Software tamper detection | + | + | + | |
Cloning protection | + | + | + | |
FIPS 140-2 level 1, compliant | + | |||
Power management | Enhanced power policy management uses 802.11 power save, and deep-sleep power modes | + | + | + |
Other | Transceiver | + | + | + |
Programmable Rx filters with events trigger mechanism | + | + | + | |
RSSI Trigger | + | + | + | |
Hostless mode | + | + | ||
Soft Roaming | + | + | ||
Agile multiband | + | + | ||
Triggered roaming | + | + | ||
Real time RSSI | + | + | ||
BLE / 2.4-GHz radio Coexistence | + | + |