SBAA541 December 2022 AMC1202 , AMC1302 , AMC1306M05 , AMC22C11 , AMC22C12 , AMC23C10 , AMC23C11 , AMC23C12 , AMC23C14 , AMC23C15 , AMC3302 , AMC3306M05
Maximum latency of the sensing stage needs to be evaluated only for point C, since point C is the closest one to the power devices. The position of this sensor allows detection of both overcurrent and short circuits but at the cost of increasing the parasitic inductances in the loop. Detection latency must be shorter than the short-circuit withstand time of the power switch and therefore depends on the switch technology. The following numbers are guidelines only. To make sure of the withstand time, refer to the device data sheets:
In addition to the latency of the overcurrent sensor, the delay of the input filter, the response time of the MCU, and the turn-off-delay of the gate driver needs to be considered. To achieve an effective turn-off delay < 1.5μs, the latency of the overcurrent sensor must be < 1μs. TI offers a line of isolated comparators with latencies < 300ns that are specifically designed for this application.