SBAA541 December 2022 AMC1202 , AMC1302 , AMC1306M05 , AMC22C11 , AMC22C12 , AMC23C10 , AMC23C11 , AMC23C12 , AMC23C14 , AMC23C15 , AMC3302 , AMC3306M05
To evaluate the maximum latency required by the AC/DC to shut down safely, system simulations were performed by applying the following conditions:
When a short-circuit is happening in the grid the converter is still switching, thus leading to uncontrolled currents. Since the fault is happening suddenly, there is not enough time for the MCU to update and correct the duty cycles. PWM updates typically happen at a fixed frequency (70 kHz or every 14.2μs in this example). By following single and double update refresh techniques, the minimum reaction time of the MCU can be 1/fs or 1/2fs. Within this time, the current in the inductor can exceed the short-circuit current rating of the power switch.
Figure 2-11 depicts the voltage and currents of the AC/DC converter. Figure 2-11 shows that in the time frame between 0ms and 19ms, the converter is operating at the nominal condition with a grid voltage equal to 400 VRMS and a current transferred from the DC to the AC. At 19ms, a short-circuit event is simulated by dropping the phase voltage to 10% of the nominal value. Simultaneously to the grid fault, the currents in the switching node start to increase due to the voltage difference between the grid and the applied one from the switching stage, as shown in Figure 2-12.
At the beginning, the current start-to-rise linearly is because the core is not saturated and is following a fixed di/dt since the inductance is nearly constant:
where
When the saturation current of the core is reached, the inductance value drops significantly, leading to a sudden increase of the current. When the real current in phase L3 reaches 30 A (overcurrent threshold), the MCU must be able to detect the overcurrent as soon as possible, since the MCU cannot detect higher currents, and shuts down before the current reaches a level above 60 A. Based on the simulation results, the current takes 4μs to reach the critical value. After this timing is reached, turn off the PWM signals as shown in Figure 2-13.
In conclusion, the system must turn off within 4µs to avoid damage to power switches. Consider the latency of the current sensing together with those of the MCU and driver stage shut down. Based on typical values of latency time of the MCU and driver stage, a maximum latency of 3.5µs must be provided by the current sensor.