SLAAE29 January 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2228 , MSPM0L2228-Q1
MSPM0 devices contain an immutable root-of-trust boot configuration routine contained in read-only memory (ROM). The boot configuration routine (BCR) is always the first code to run on the Cortex-M0+ processor following a BOOTRST of the device. The BCR also runs upon software invocation of the bootstrap loader (BSL) as it is needed for authorizing the BSL entry. The core responsibilities of the BCR are to:
During execution of the BCR, the AHB-AP, ET-AP, and PWR-AP DAPs remain inaccessible through the SWD interface. If the user specified security policy allows debug access to the device, then these DAPs will become available when the hardware starts the user application or the bootstrap loader.