SLAAE29 January 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
MSPM0 devices contain a dedicated region of flash memory for storing user-specified security and device configuration policies. This region is referred to as the NONMAIN flash region. The boot configuration routine (BCR) and bootstrap loader (BSL) reference the user-specified data stored in the NONMAIN flash region to configure the device for operation.
The user must provision the NONMAIN flash memory region of the device with the desired policies during production. This section will introduce the security policies which are user configurable through the NONMAIN configuration memory.
The NONMAIN flash region is partitioned into two distinct data structures:
Both data structures are backed by their own 32-bit CRC digests, which are used as a part of the configuration data error resistance scheme.