SLAAE29 January 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
MSPM0 devices may also contain an immutable bootstrap loader (BSL) in read-only memory (ROM). The BSL provides a means to program and verify the contents of the device memory through a standard serial interface (UART or I2C), as opposed to the serial wire debug (SWD) interface.
The BSL can only be started by the BCR. The BCR checks for a valid BSL invoke condition (software invoke, IO pin invoke, blank device invoke) and validates that the BSL is enabled for use before starting the BSL. When the BSL exits, the BCR runs again to load the current device security policies and start the user application.
The BSL is always protected by a 256-bit user-specified password that must be passed to the BSL through the UART or I2C interface when starting a BSL session. The BSL can be disabled if it is not used (see the BSL enable/disable policy).