SLAAE29 January 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
The BCR supports checking the data integrity of a user-specified address range in the MAIN flash memory before transferring execution from the BCR (in ROM) to the user application (in MAIN flash memory).
Purpose
The integrity check may be used as an additional step to ensure the code which runs first after the boot ROM (usually the secure boot image manager) has a CRC digest that matches the expected value. This integrity check reduces the likelihood that any unexpected corruption of critical code in the flash memory (which may be responsible for authenticating the remaining user application software image) can create a security vulnerability.
Capabilities
A start address, length, and ISO-3309 CRC-32 digest may be provisioned into the NONMAIN configuration memory. During the boot process, the BCR will compute the CRC-32 digest of the specified range in the MAIN flash memory, and verify the computed digest against the provisioned (expected) digest. If the values match, the user application is started. If the values do not match, the user application is not started and the result is a catastrophic boot error.