SLAAE56A November 2022 – March 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
Similar to STM32G0 devices, MSPM0 devices have a minimum operating voltage and have modules in place to make sure that the device starts up properly by holding the device or portions of the device in a reset state. Table 3-4 shows a comparison on how this is done between the two families and what modules control the power up process and reset across the families.
STM32G0 Devices | MSPM0 Devices | ||
---|---|---|---|
Modules governing power up and resets | PWR (power) and RCC (Reset and Clock Control) modules | Module governing power up and resets | PMCU (Power Management and Clock Unit) |
Voltage-Level Based Resets | |||
POR (Power-On Reset) | Complete device reset. First level voltage release for power up. Lowest voltage level for power down. | POR (Power-On Reset) | Complete device reset. First level voltage release for power up. Lowest voltage level for power down. |
BOR (Brownout Reset) with configurable levels | Sometimes programmable. Set voltage level that releases reset state on power up, or resets device on power down. | Configurable BOR (Brownout Reset) | Can be configured as a reset or interrupt, with different voltage thresholds, combining the functionality of the STM32G0 BOR and PVD. |
PVD (Programmable Voltage Detector) | Configurable voltage monitor that can provide interrupts. |
STM32G0 defines different reset domains, while MSPM0 devices have different levels of reset states. For MSPM0 devices, the reset levels have a set order, and when a level is triggered, all subsequent levels are reset until the device is released into RUN mode. Table 3-5 gives a brief description and comparison between STM32G0 reset domains and MSPM0 reset states. #GUID-D14F0E25-5973-4349-9966-B9316B34CA29 shows the relationship between all of the MSPM0 reset states.
STM32G0 Reset Domains |
MSPM0 Reset States#LI_MPK_FWV_HVB |
||
---|---|---|---|
Power reset domain | Typical triggers are POR, BOR, and exits from standby or shutdown modes. All registers reset except those outside VCORE domain. | POR | Typical triggers: POR voltage levels, SW trigger, NRST held low for >1s. Resets shutdown memory, re-enables NRST and SWD, triggers BOR |
BOR | Typical triggers: POR or BOR voltage level, exit from shutdown mode. Resets PMU, VCORE, and associated logic. Triggers BOOTRST. | ||
No exact equivalent. Boot configuration is read on the fourth clock cycle of SYSCLK after a reset. | Boot reset (BOOTRST) | Typical triggers: BOR or software trigger, fatal clock failure, NRST held low for <1 s. Executes boot configuration routine. Resets majority of core logic and registers, including RTC, clock, and IO configurations.#LI_GB2_GWV_HVB SRAM power cycled and lost. Triggers SYSRST. | |
System reset domain | System reset sets all registers to their reset values except the reset flags in the clock control and status register (RCC_CSR) and the registers in the RTC domain. | System reset (SYSRST) | Typical triggers: BOOTRST, BSL entry or exit, watchdog timer, software trigger, debug subsystem. Resets CPU state and all peripherals except RTC, LFCLK, LFXT, and SYSOSC frequency correction loop. Device enters RUN mode on exit. |
No equivalent | CPU-only reset (CPURST) | Software and debug subsystem triggers only. Resets CPU logic only. Peripheral state are not affected. | |
RTC domain | Triggered by software or VDD or VBAT power on, if both supplies where previously been powered off. Resets only the LSE oscillator, RTC, backup registers and RCC RTC domain control register. | RTC and associated clocks are reset through BOOTRST, BOR, or POR.#LI_GB2_GWV_HVB |