SLAU847D October 2022 – May 2024 MSPM0L1105 , MSPM0L1106 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2228 , MSPM0L2228-Q1
Operations on the flash memory are executed by configuring the CMDTYPE and CMDCTL registers for the desired command, along with any other registers which must be configured for a particular command, and writing 0x01 to the CMDEXEC register to initiate the command.
When 0x01 is set in CMDEXEC, the commanded operation begins executing. While an operation is executing, most configuration registers are blocked for writes until the operation completes. Some registers (for example, mask registers) can change state under hardware control while the operation runs to completion. The flash controller indicates completion of the commanded operation by setting the CMDDONE bit in the STATCMD register. The flash controller also sources an interrupt vector to the CPU subsystem to indicate a “DONE” status when an operation has completed.
The software sequence of setting the CMDEXEC bit and waiting for the CMDDONE response must be executed from either the device SRAM or from a different flash bank from the bank that is being operated on, as the flash controller will take control of the flash bank undergoing the operation. Reads to the flash bank that is being operated on while the flash controller is executing the command are not predictable.
The flash controller provides five basic commands for operating on the flash memory, specified in the COMMAND field of the CMDTYPE register. These commands are described in Table 6-4.
Command | Description |
---|---|
NOOP | No operation (default setting). |
PROGRAM | Selects a program operation on the flash memory. |
ERASE | Selects an erase operation on the flash memory. |
READVERIFY | Selects a standalone read verify operation. |
BLANKVERIFY | Selects a standalone blank verify operation. |