SLAU887 February 2023 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The MSPM0 Bootloader (also known as BSL) provides a method to program and verify the device memory (Flash and RAM) through a standard serial interface (UART or I2C).
All trademarks are the property of their respective owners.
The bootstrap loader (BSL) provides a method to program or verify the device memory through a standard UART or I2C serial interface.
Key features of the BSL that are accessible through the serial interface include:
Bootloader (BSL) - Boot routine used to load data to the device memory
Bootcode (BCR) - Startup Routine that runs after BOOTRST, to configure the device for executing application
BCR configuration - Configuration structure that contains all user configurable parameters for Bootcode, which resides in Non-main flash memory
BSL configuration - Configuration structure that contains all user configurable parameters for Bootloader, which resides in Non-main flash memory