Inner vias must be placed close to the traces and not in the absolute center of the inductor — this reduces the parasitic resistance.
Keep the inner 30% of the sensor area unwound for most applications, but for inductive metal button replacement, place as many turns as possible.
The sensor capacitor must be placed as close as possible to the sensor to minimize the RS of the traces. Note that this rule does not apply to LDC0851, LDC2112, LDC2114, and LDC3114 devices. For these devices, place the sensor capacitor close to the corresponding device pin.
Use thicker traces between the inductor and capacitor when possible. Typically 10 mil (0.25 mm) is sufficient.
Do not use a ferrite bead as a sensor inductor — it does not generate a magnetic field effective for LDC applications.