SNOAA35F April 2019 – December 2024 LM2901 , LM2901B , LM2901B-Q1 , LM2903 , LM2903-Q1 , LM2903B , LM2903B-Q1 , LM339 , LM339-N , LM393 , LM393-N , LM393B , LM397 , TL331 , TL331-Q1 , TL331B
For both used and unused comparators, the inputs must not be connected directly to ground or any other low impedance node. Always add some resistance to limit the current to less than 10mA, regardless of any possible fault condition. All the input pins have a diode from the input to the device’s GND, or V–, pin. In dual supply applications, the GND pin is the most negative. However, during power up, power down, or supply faults, the GND pin can become positive. If this occurs then a grounded input pin can have potentially damaging current flow due to the input diode. Even if the GND pin is also grounded, such as in single supply applications, there is a possibility that the input ground can be negative relative to the op amp’s internal ground node. Ground differences occur when there is poor layout or high current transients, ∆I/∆t. Adding 1kΩ to 10kΩ series resistors to the input pin is acceptable in most applications.