SBAA275A June 2018 – March 2023 ADS1120 , ADS112C04 , ADS112U04 , ADS1147 , ADS1148 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1220 , ADS122C04 , ADS122U04 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS125H02 , ADS1260 , ADS1261 , ADS1262 , ADS1263
The two-wire measurement topology is the same as shown in the two-wire RTD design in Section 2.2. One IDAC sources current from AIN0 into the reference resistor RREF. Then the current flows into the first RTD connection measured by AIN1. The RTD is attached to and measured from AIN1 to AIN4. The IDAC current is then shunted into the bias resistor RBIAS.
For the two-wire RTD measurement, the lead resistance of the RTD is an error term that cannot be removed.