SBAA275A June 2018 – March 2023 ADS1120 , ADS112C04 , ADS112U04 , ADS1147 , ADS1148 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1220 , ADS122C04 , ADS122U04 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS125H02 , ADS1260 , ADS1261 , ADS1262 , ADS1263
This design should be exactly the same as in the two-wire RTD design in Section 2.1. The IDAC current is being routed through an alternate input and measurements are taken from AIN1 and AIN2. However, the considerations in reference resistor size, IDAC current, reference voltage, and PGA input voltage are exactly the same.
The measurement circuit requires:
To verify that the design is within the ADC range of operation, Calculate the voltages for AIN1 and AIN2 and the maximum differential input voltage. Verify that VAIN1 and VAIN2 are within the input range of the PGA given the gain setting and supply voltage. Use the maximum RTD resistance based on the desired temperature measurement.
Additionally, verify that the voltage seen at the IDAC pin (where VAIN0 = VAIN1) is within the current source compliance voltage. When the IDAC output voltage rises too close to AVDD, the IDAC loses compliance and the excitation current is reduced.
The reference resistor, RREF must be a precision resistor with high accuracy and low drift. Any error in the RREF reflects the same error in the RTD measurement. The REFP0 and REFN0 pins are shown connecting to the RREF resistor as a Kelvin connection to get the best measurement of the reference voltage. This eliminates any series resistance as an error from the reference resistance measurement.