SNVAA44 july   2023 LM5155 , LM5155-Q1 , LM51551 , LM51551-Q1 , LM5156 , LM5156-Q1 , LM51561 , LM51561-Q1 , LM5157 , LM5157-Q1 , LM51571-Q1 , LM5158 , LM5158-Q1 , LM51581

 

  1.   1
  2.   How to Implement the Soft Start in a Flyback
  3.   Trademarks
  4. 1Overview
  5. 2Design Considerations
  6. 3Soft-Start Time Calculation Considerations
    1. 3.1 Soft-Start Capacitor Selection for the LM5155x
  7. 4Soft-Start Time Within Different Topologies
    1. 4.1 Buck Topology
    2. 4.2 Boost Topology
    3. 4.3 Sepic Topology
    4. 4.4 Flyback Topologies
      1. 4.4.1 PSR Flyback: Bipolar Transistor as Pull Down for COMP Pin
      2. 4.4.2 Secondary Side Soft-Start Components
  8. 5Fixing Soft-Start Issue
  9. 6Summary
  10. 7References

Design Considerations

To define an appropriate soft-start time to ramp up the output voltage to the required level some aspects of the application need to be considered:

  • Maximum output current
  • This is the maximum load current which the converter can supply without getting into any limitation, either current limit or device parameter limits. Device parameter limits must never be violated and a well-defined margin need to be considered.
  • Output capacitance and the ESR of the output capacitors. The capacitance plays a significant role as it dictates the value of the inrush current, together with the target value of the output voltage. This current is basically only limited by the ESR of the capacitors. (In most cases the ESR can be neglected as, especially for ceramic capacitors, it is quite low.)
  • Behavior of the load during the startup phase
  • Beside the inrush current of the output capacitor also the load on the SMPS can contribute to the current during the start phase. This needs to be evaluated and considered individually, for example, an ohmic load can ramp linear while a Processor or uController can only start at a certain voltage level or even after the power supply has stabilized and, in this case, might not need to be considered for the soft-start time.