DLPA059H January 2015 – April 2024 DLP160AP , DLP160CP , DLP2000 , DLP2010 , DLP230NP , DLP3010 , DLP3310 , DLP470NE , DLP470TE , DLP4710 , DLP471NE , DLP471TE , DLP471TP , DLP480RE , DLP550HE , DLP550JE , DLP650LE , DLP650NE , DLP650TE , DLP651NE , DLP660TE , DLP670RE , DLP780NE , DLP780TE , DLP781NE , DLP781TE , DLP800RE , DLP801RE , DLP801XE , DLPA1000 , DLPA2000 , DLPA2005 , DLPA3000 , DLPA3005 , DLPC2607 , DLPC3420 , DLPC3421 , DLPC3430 , DLPC3433 , DLPC3435 , DLPC3438 , DLPC3439 , DLPC6401 , DLPC6540
The electronics portion of the display system starts with a video input signal (for example, 12/16/18/24-bit RGB (red, green, blue) parallel, DSI, FPD-Link or Vx1 interfaces, typically driven by an application or media processor. The output of the electronics portion includes video signal to the DMD commonly using low voltage differential signaling (LVDS) or Sub-LVDS, illumination drive, and power. Figure 4-2 shows an example of the electronics hardware.
Table 4-2 includes the components of the electronics portion of the display system.
Component | Description |
---|---|
Applications processor | The function of the applications processor is to deliver the video signal to the DLP display system as well as inter-integrated circuit (I2C) interface to provide command and control functions. Any video-capable processor should be able to handle this task. |
Display controller | The DLP display
controller is the digital interface between the DMD and the rest of
the system. The controller takes digital input from an applications
processor and drives the DMD over a high speed interface. The DLP
controller also generates the necessary signals (data, protocols,
timings) required to display images on the DMD. Each display controller has a software user’s guide that details all its supported video handling functions, which will vary depending on the DLP chipset selected. To see an example software programmer’s guide for the .47 1080p DLP Pico chipset (DLP4710), see the DLPC3439 Software Programmer’s Guide. Video signal inputs
DMD signal outputs
The display controllers support image processing that helps optimize the image quality displayed, including data compression. A DLP Light Control chipset should be used if precise pixel to pixel mapping is required (typically used in structured lighting applications, learn more here). Image processing features depending on the chipset could include TI DLP® IntelliBright™ Algorithms for the DLPC343x Controller, DLP BrilliantColor™ technology, image keystone correction, warping, blending, frame rate conversion, integrated support for 3-D displays and more. Some systems require dual controllers to format the incoming data before sending it to the DMD. The DMD and its appropriate controller are required to be used together in a system design to ensure reliable operation. |
FPGA | Some chipsets
incorporate a technology which creates either two or four pixel
images on the screen from a single DMD micromirror. This is
accomplished through a combination of proprietary image processing
coupled with an optical actuator. The actuator is an opto-mechanical
element which is positioned in the optical path between the DMD and
the projection lens, and which has the ability to slightly alter the
direction of the projection light rays. A 2-way actuator can direct
light into two discrete directions, and a 4-way actuator can direct
light into four discrete directions. The proprietary image
processing converts the image data (from the customers application
processor) into either two or four sub-frames of data. These
sub-frames of data are then displayed on the DMD, synchronized with
the direction-state of the actuator. For chipsets which incorporate
this technology, the image processing is performed in an FPGA which
sits in the data path between the customers application processor
and the DLP controller. This FPGA is designed to receive data in the
same manner that a DLP controller would, and generate both the
sub-frame data as well as actuator control signals:
|
PMIC, LED drive, and motor driver | In most cases, a DLP
PMIC is responsible for providing input power to the DLP display
controller, DMD, and LED illumination components. The PMIC takes
care of supplying core voltages related to the DLP chipset and
gently power sequencing the DMD to ensure correct operation. It also provides other monitoring and protection functions, and dynamic LED control based on image color content (for example, TI DLP® IntelliBright™ Algorithms for the DLPC343x Controller). Integration of the power supply and LED driver circuitry in a small IC not only allows for small-size electronics to be designed, but also reduces the product design cycle time. A motor driver is also needed for systems that include a color wheel. This capability provides a color wheel motor drive control for phosphor laser illumination-based applications, as well as switching regulators and adjustable linear regulators for customer designed peripherals. It supports two peripherals by supplying three fan drivers and one 3-phase Back electromotive force (BEMF): motor driver or controller for a color wheel. |
Flash memory | Application-specific configurations are stored in the Flash memory. This component is typically placed on the electronics board or the DMD flex cable. |
DLP display controller and PMIC that accompany the DLP Pico DMDs are very small enabling extremely compact display products. Figure 4-3 shows both sides of an example printed circuit board design (estimate only) with the DLPA2000 PMIC and the DLPC3430 controller device, which drives a .2 WVGA (DLP2010) DMD.