SLUAAO5B January   2023  – August 2024 TPS561243 , TPS561246 , TPS562202 , TPS562203 , TPS562206 , TPS562207 , TPS562242 , TPS562243 , TPS562246 , TPS563202 , TPS563203 , TPS563206 , TPS563207 , TPS563252 , TPS563257 , TPS564242 , TPS564247 , TPS564252 , TPS564255 , TPS564257 , TPS565242 , TPS565247 , TPS566242 , TPS566247

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Comparison of Pinout
  6. 3Schematic Diagram
    1. 3.1 How to Co-layout Among Three Types of SOT-563
    2. 3.2 How to Co-Layout Between TPS56x252/7 and TPS56x242/7
    3. 3.3 How to Co-layout Between TPS56x252/7 and TPS56x203/6
    4. 3.4 How to Co-Layout Between TPS56x242/7 and TPS56x203/6
  7. 4Experimental Results
  8. 5Summary
  9. 6References
  10. 7Revision History

Comparison of Pinout

The TPS56x243/6 and TPS56x203/6 pinout with SOT-563 package is shown in Figure 2-1. TPS56x243/6 and TPS56x203/6 pinout is quite common in the industry. The TPS56x242/7 pinout with SOT-563 package, which has been optimized is shown in Figure 2-2. This pinout integrates BST capacitor and adds AGND for pin 4.The TPS56x252/7 pinout with SOT-563 package is shown in Figure 2-3. This pinout integrates BST capacitor and add PG for pin 4. These three device families have the same pin functionality aside from pin 4 as shown in Table 2-1. With compatible external circuitry, co-layout can be achieved for the three packages.

 TPS56x243/6 and TPS56x203/6 PinoutFigure 2-1 TPS56x243/6 and TPS56x203/6 Pinout
 TPS56x242/7 PinoutFigure 2-2 TPS56x242/7 Pinout
 TPS56x252/7
                                        Pinout Figure 2-3 TPS56x252/7 Pinout
Table 2-1 Pin Functions
Pin Description
No. Name
1 VIN Input voltage supply pin. Connect the input decoupling capacitors between VIN and GND.
2 SW Switch node pin. Connect the output inductor to this pin.
3 GND GND pin source terminal of the low-side power NFET as well as the ground terminal for controller circuit.
4 PG Open-drain power-good indicator.
AGND Ground of the internal analog circuitry. Connect AGND to the GND plane.
BST Supply input for the high-side NFET gate driver circuit. Connect 0.1-uF capacitor between BST and SW pins.
5 EN Enable input control. Driving EN high enables the converter.
6 FB Converter feedback input. Connect to the output voltage with a feedback resistor divider.