SLYY204C January 2021 – February 2024 AMC1300 , AMC1302 , AMC1302-Q1 , AMC1305M25-Q1 , AMC1311 , AMC1311-Q1 , AMC131M03-Q1 , AMC1336 , AMC1336-Q1 , AMC1350 , AMC1411 , AMC3301 , AMC3301-Q1 , AMC3330 , AMC3330-Q1 , AMC3336 , AMC3336-Q1 , ISOW1044 , ISOW1412 , ISOW7741 , ISOW7840 , ISOW7841 , ISOW7841A-Q1 , ISOW7842 , ISOW7843 , ISOW7844 , UCC12040 , UCC12041-Q1 , UCC12050 , UCC12051-Q1 , UCC14130-Q1 , UCC14131-Q1 , UCC14140-Q1 , UCC14141-Q1 , UCC14240-Q1 , UCC14241-Q1 , UCC14340-Q1 , UCC14341-Q1 , UCC15240-Q1 , UCC15241-Q1 , UCC21222-Q1 , UCC21530-Q1 , UCC21540 , UCC21710-Q1 , UCC21750-Q1 , UCC23513 , UCC25800-Q1 , UCC5870-Q1
There is much to consider when constructing a reliable isolation barrier in a system, including the isolation rating, creepage and clearance distance, CMTI, and EMI.
Functional, basic and reinforced isolation refer to the insulation rating level assigned to an electrical system, as listed in Table 1.
Insulator rating | Description |
---|---|
Functional | Insulation necessary for the correct operation of the equipment |
Basic | Insulation that provides basic protection against electric shock |
Supplementary | Independent insulation applied – in addition to basic insulation – to protect against electric shock in the event of a failure of the basic insulation |
Double | Insulation comprising both basic and supplementary insulation |
Reinforced | A single insulation system that provides a degree of protection against electric shock equivalent to double insulation |
Functional isolation refers to the minimum amount of isolation assigned to a system so that it will function properly, without necessarily protecting against electrical shock. One example of functional isolation is proper printed circuit board (PCB) conductor spacing for a given voltage rating.
Basic isolation provides “sufficient” protection against electrical shock, with a safety rating at parity with the highest system-level voltage.
Reinforced isolation is the highest commercial rating applied to high-voltage systems. One way to meet reinforced isolation requirements is to introduce further distance across the isolation barrier such that it can withstand higher-voltage testing standards and a longer rated lifetime. For example, in International Electrotechnical Commission (IEC) 60747-17 and IEC 607475-5, the mandatory partial discharge test voltage (VPD) is held to a higher standard for reinforced isolation compared to basic isolation. Learn more about reinforced isolation in the What is Reinforced Isolation? video.
Certifying a high-voltage system for reinforced isolation begins by selecting isolators compliant with safety and certification testing protocols, as defined by various committees. Underwriters Laboratories (UL) is a global safety certification lab in the United States, but different countries regulate compliance to their local or regional system standards. Thus, isolators intended for global use must comply with various international safety standards.
Table 2 summarizes IEC standard requirements for digital (capacitive and magnetic) isolators and optocouplers.
Test | IEC 60747-17 capacitive and magnetic isolators |
IEC 60747-5-5 optocouplers |
|
---|---|---|---|
Basic isolation | Reinforced isolation | Reinforced isolation only | |
VIORM – maximum repetitive peak isolation voltage | AC voltage (bipolar) | AC voltage (bipolar) | AC voltage (bipolar) |
VIOWM – maximum working isolation voltage | AC voltage based on time-dependent dielectric breakdown (TDDB) | AC voltage based on TDDB | Based on partial discharge test |
VPD – partial discharge test voltage | VTEST = 1.5 × VIOWM | VTEST = 1.875 × VIOWM | VTEST = 1.875 × VIOWM |
VIOSM – maximum surge isolation voltage | VTEST = 1.3 × VIMP | VTEST = 1.6 × VIMP10 kVPK (minimum) | 10 kVPK (minimum) |
Minimum rated lifetime | 20 years × 1.2 | 20 years × 1.5 | Not defined |
Failure rate over lifetime | 1,000 ppm | 1 ppm | Not defined |
Allowable isolation materials | Silicon dioxide (SiO2) and thin-film polymer | SiO2 and thin-film polymer | Not defined |
Isolators have several important parameters. The creepage and clearance distance, for example, is the shortest distance between two conductive leads across the isolation barrier. As shown in Figure 3, creepage distance is the shortest distance measured between adjacent conductors across the surface of an IC package, whereas clearance distance is measured through the air.
Package technology plays an important role in achieving higher measures of creepage and clearance distance by providing different options for engineers. High-quality mold compounds, wide-body packages and higher reinforced isolation ratings must complement each other, because higher isolation ratings need wider packages and better mold compounds so that packages don’t cause breakdown and arcing.
Another parameter is CMTI, which indicates an isolator’s ability to operate reliably in the presence of high-speed transients and is measured in kilovolts per microsecond or volts per nanosecond. The proliferation of wide band-gap semiconductors has resulted in higher transient voltage (dV/dt) edge rates, making the measure of CMTI critical for gauging an isolator’s resiliency. High-performance isolators have CMTI ratings easily reaching 100 V/ns, and many are tested in excess of 200 V/ns. A low CMTI isolator operating in a high dV/dt environment can expect to have signal integrity problems such as pulse jitter, distortion, erratic operation or missing pulse information.
Isolation trade-offs are similar at the IC and system level. Smaller IC package sizes, higher integration, thermal management and compliance with certification standards often compete against the need to reduce EMI and achieve higher efficiency. Selecting isolated components designed to meet all of these needs at the IC level helps facilitate a seamless transition to fully reinforced compliance at the system level.