This document describes the preparation and usage of the sample code for the LP589x(-Q1)/TLC698x device family when paired with a LAUCHXL-F280039C. Following the instructions provided for setup, the installed code lights up the LEDs on the EVM. The LP5890/1/2(-Q1) devices can be paired with the LP5899(-Q1) to use a standard SPI module of the MCU to communicate to the LED drivers. Moreover, the TLC6983/4 devices can be paired with the TLC6989 to use a standard SPI module of the MCU to communicate to the LED drivers.