There are two sets of switchover methods that power MUX solutions fall under:
- Break-before-make method occurs when the switch for the first supply completely turns off before the second supply switch is turned on.
- This prevents reverse current flow from one supply to another.
- There is a period of time where no power is being delivered from the supply to the output. This is known as the switchover time, or tSW.
- Diode mode is a make-before-break method where the diode or switch for the first supply remains on while the second supply switch is turned on. Reverse current is then prevented by the presence of a diode or a device which detects the reverse current flow and shuts off a corresponding FET (such as our eFuse, Ideal Diode or ORing controllers).
- The benefit of this approach is minimal output voltage drop, as power is continuously supplied to the load.
- The tradeoff depends on what diode device is used:
- Schottky or Silicon diode will result in power dissipation and voltage drop during normal operation.
- eFuse, ORing or Ideal diode controller methods will result in some level of reverse current flow, potentially significant or insignificant depending on the application.