• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Using the Filters with the DC/DC Step-Down Converter

    • SLVAFE0 February   2023 TPS62441-Q1 , TPS62442-Q1 , TPS62810-Q1 , TPS62811-Q1 , TPS62812-Q1 , TPS62813-Q1 , TPS628501-Q1 , TPS628502-Q1 , TPS628503-Q1 , TPS62870 , TPS62870-Q1 , TPS62871 , TPS62871-Q1 , TPS62872 , TPS62872-Q1 , TPS62873 , TPS62873-Q1 , TPS62874-Q1 , TPS62875-Q1 , TPS62876-Q1 , TPS62877-Q1 , TPSM8287A06 , TPSM8287A10 , TPSM8287A12 , TPSM8287A15

       

  • CONTENTS
  • SEARCH
  • Using the Filters with the DC/DC Step-Down Converter
  1.   Abstract
  2.   Trademarks
  3. 1Overview
  4. 2Detailed Description
    1. 2.1 Input Filter Design
    2. 2.2 Output Filter Design (Second Stage)
  5. 3Measurement and Analysis
  6. 4Damping of the Filters
  7. 5Further Analysis with Damped Filters
  8. 6Conclusion
  9. 7Reference
  10. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Using the Filters with the DC/DC Step-Down Converter

1 Abstract

The efficient design of a power delivery network PDN is a challenging task because all the segments of PDN are linked with each other. Changes in one component can have a significant influence on all the other components. This application note focuses on designing of filters and also discusses the stability problems caused by adding the input filter or the second stage of output LC filter if they are not designed properly by keeping a look on certain important parameters. Furthermore, the application note also explains the damping methods for resolving the stability issues caused by the addition of filters with step-down converter.

Trademarks

All trademarks are the property of their respective owners.

1 Overview

The second-order low-pass LC filter is the most commonly used filter type with DC/DC converters. The filter is used to suppress high-frequency noise or minimize the output voltage ripple. After the addition of the filters on the input and the output sides, the overall output impedance of the DC/DC converter shows high resonance peaks if the filters are undamped. When the load draws current, the voltage at the output can vary due to these resonance peaks in the impedance curve. One other concern is that if the resonant frequency of the filter is in the range of the crossover frequency of the control loop, it affects the control loop stability which further affects the transient behavior of the device. DC/DC converter acts as a load for the input filter which provides negative variable resistance. When this negative dynamic resistance is connected to the input filter, it acts as a negative oscillator circuit. It causes system instability in the case of an undamped system.

This application note discusses in detail how one can design the input and second order LC filter for DC/DC converter and which parameters are important to keep in mind while designing them. TPS6281x -Q1 is used as an example in this application note.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale