SLVAFE0 February 2023 TPS62441-Q1 , TPS62442-Q1 , TPS62810-Q1 , TPS62811-Q1 , TPS62812-Q1 , TPS62813-Q1 , TPS628501-Q1 , TPS628502-Q1 , TPS628503-Q1 , TPS62870 , TPS62870-Q1 , TPS62871 , TPS62871-Q1 , TPS62872 , TPS62872-Q1 , TPS62873 , TPS62873-Q1 , TPS62874-Q1 , TPS62875-Q1 , TPS62876-Q1 , TPS62877-Q1 , TPSM8287A06 , TPSM8287A10 , TPSM8287A12 , TPSM8287A15
The output impedance, bode plot and load transient response of the converter are again measured after adding the parallel damping branch (Rd-Cd) with the filters.
In Figure 5-1, it can be seen that addition of the damping with the filters has helped to reduce the peak in the output impedance curve and reduces the maximum impedance value to 0.15 Ω. This damping method helps to reduce the excessive power loss also as compared to series Rd with filter as shown in Figure 4-1(b). In Figure 5-2, phase margin is also improved to 45.9° from 26° by damping the filters. Figure 5-3 shows the transient response of the device in which oscillations are properly damped. Therefore, it can be observed that the addition of the damping branch to the filters helps to dampen the filter resonance, which improves the phase margin. Furthermore, the load transient response also appears to be reasonable as compared to the transient response of the system with undamped filters.