SPRADJ8 October 2024 AM3351 , AM3352 , AM3354 , AM3356 , AM3357 , AM3358 , AM3359 , AM4372 , AM4376 , AM4377 , AM4378 , AM4379 , AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442 , DP83822H , DP83822HF , DP83822I , DP83822IF , DP83826E , DP83826I , DP83848-EP , DP83848Q-Q1 , DP83867CR , DP83867CS , DP83867E , DP83867IR , DP83867IS , DP83TC812R-Q1 , DP83TC812S-Q1 , DP83TC813R-Q1 , DP83TC813S-Q1 , DP83TC814R-Q1 , DP83TC814S-Q1 , DP83TG720R-Q1 , DP83TG720S-Q1 , DP83TG721R-Q1 , DP83TG721S-Q1
To initiate traffic using utility tools such as
ping
or iperf
, set an IPv4
address. This can be done with a DHCP server to assign dynamic IP addresses or done
manually with static IP addresses. When using the static method and a direct
connection topology, both link partners need an IP address manually assigned to the
same subnet. For example, if the IPv4 address is 192.168.1.1 with a netmask of 24,
then the first three set of numbers (that is, 192.168.1.x) is the subnet. Section 11 has an example
of how to set static IP addresses at runtime.