SLVAF66 June 2021 DRV3255-Q1 , DRV8300 , DRV8301 , DRV8302 , DRV8303 , DRV8304 , DRV8305 , DRV8305-Q1 , DRV8306 , DRV8307 , DRV8308 , DRV8320 , DRV8320R , DRV8323 , DRV8323R , DRV8340-Q1 , DRV8343-Q1 , DRV8350 , DRV8350F , DRV8350R , DRV8353 , DRV8353F , DRV8353R
If the VDS monitors or other current protection recognizes an overcurrent event, the obvious solution is to turn off the FETs so they stop current from passing through. In this scenario, the phase current could be more than 10 or 100 times higher than the typical use case. As already explored in Section 2, more current in the phase results in higher parasitic inductive spiking, but increasing the FETs rise or fall time by decreasing the gate drive current decreases the inductive spiking.
In a typical gate-driver case, Section 3.1.2.2 established the sink current is fixed by the external gate resistors and cannot be changed during the overcurrent event. However, TI’s Smart Gate Drive technology automatically lowers the gate drive current so that the FET has a longer fall time than the typical value, which reduces the overall voltage spiking that occurs from an overcurrent event.