SLVAF66 June 2021 DRV3255-Q1 , DRV8300 , DRV8301 , DRV8302 , DRV8303 , DRV8304 , DRV8305 , DRV8305-Q1 , DRV8306 , DRV8307 , DRV8308 , DRV8320 , DRV8320R , DRV8323 , DRV8323R , DRV8340-Q1 , DRV8343-Q1 , DRV8350 , DRV8350F , DRV8350R , DRV8353 , DRV8353F , DRV8353R
As previously mentioned, the MOSFET drain and gate current is the backbone of power delivery to the motor. To deliver current and turn the FET on, charge must build up on the intrinsic gate capacitors of the MOSFET. This process is explained in more detail in the Fundamentals of MOSFET and IGBT Gate Driver Circuits and Understanding Smart Gate Drive application notes.
As a result, link the rate of electrical charge, or current, at the gate-to-the rise in drain-to-source voltage of the FET, as shown in the ideal first-order Equation 1:
Where:
According to Equation 1, a high IDRIVE and a small Qgd results in a very fast slew rate, as VDRAIN is usually fixed in a system unless the system supply voltage is specifically designed to change. Since a high slew rate results in lower switching losses in the MOSFETs it can seem at first beneficial to make the slew rate as high as possible. However, most designers try to use a higher slew rate without realizing that there are adverse effects of using a slew rate that is too high for the design.