Figure 8-2 Example Smart Gate Drive
Schematic Accounting for Parasitics
When PCBs are manufactured, physics dictates that
some more resistors, inductors, and capacitors are added to the system. These added
components are the result of parasitics - an example is illustrated in Figure 8-2.
One of the primary goals of layout is
to minimize these parasitics so they are effectively negligible. What makes high
power design difficult is that more current and voltage makes the effects of these
parasitics more pronounced.
However, additional bullet points
have been added here to help in the context of the high-power gate driver devices
offered by TI:
Actual PCBAs have parasitic
components that are added to the system
Long traces add
capacitance and resistance
Thin traces also add
resistance and inductance
10 mil/A with 1-oz copper pour is a guideline for
the trace width but it also applies to vias, specifically angular ring area.
The larger or wider the traces and vias are, the less inductance.
As such, use at least 15
mil gate current source and sink paths, but 20 mil is preferred
Note: The 10 mil/A with
1-oz copper guideline starts to break and wider traces are required
as a result of heat within the middle layers
To get better thermal and current
capability it is recommended to provide the VDC, motor phases, and GND power
polygons in the external layers and, if possible, repeat the polygons in
internal layers as well
Making sections of a trace
thinner and smaller in the same trace adds impedance mismatch
Use teardrops or planes
to smooth out the mismatch
More current means higher voltage
spiking due to the parasitic effects
Component footprints, in addition
to the components, add parasitics
Vias in the path add parasitics,
namely inductance
The return path must be
understood:
DC current spreads out
on the GND planes as far as it can go, whereas high-frequency current
gravitates underneath the corresponding high-speed trace. This is why
common GND, as opposed to split GND, is always better unless current
needs to be diverted from flowing in a certain area of the board.
Common ground is always better
than split GND from a parasitic perspective. Split GND is only ever used to
divert high-frequency current as well as large amounts of current away from the
sensitive components. That means that these signals must be traveling towards or
near those components to warrant a split GND.
If a split GND is chosen,
then know inductance is added to some paths
For additional understanding,
imagine that you are the current: draw the loop from the source of the pin or
component to the GND pin of the device or external connector. Make the loop as
small as possible. This sometimes means adding lots of vias in the planes,
increasing ground plane coverage, or rearranging components.
Experience shows that the price
difference between 100 and 300 GND stitching vias is negligible in PCB
manufacturing. Create a plane of GND stitching vias to connect outer- and
inner-layer GNDs.
Manually place GND
stitching vias where the automated tools fail
The most important signals and
component locations on a typical gate driver IC are included in the following
list, in descending order of importance:
Voltage regulators and their
associated capacitors (like VCP, VGLS, or low-voltage regulators AVDD, DVDD, and
so forth) (most critical)
Bypass capacitors for input
supplies and reference voltages (like VM, GND, and CSAREF)
Signal path and higher current or
power paths (like GHx, GLx, and SHx)
Digital signals that switch
often, ordered by frequency (like SPI or PWM signals)
Digital signals that do not
switch often (like ENABLE or nFAULT) (least critical)