High power motor applications can range anywhere from lower voltage systems that result in hundreds of watts, such as a 12-V automotive power seats, to multiple kilowatt systems, such as 60-V and 100-A power tools. Typically, these systems use shunt-based current sensing, and non-isolated gate drivers that control large power MOSFETs. While these applications can be powered from a battery or gridded AC power converted to DC, they all have the common goals to be robust and protected against high current and high voltage events that result from shoot-through, short-circuit, overcurrent, MOSFET reverse recovery, or PCB parasitic inductance behavior.
For example, power tools have high power ratings for industrial and household purposes, such as drilling, grinding, cutting, polishing, driving fasteners, and more. Requirements include:
When designing high power systems, these requirements produce tradeoffs and conflict with each other. In the case of power tools, high current, efficiency, and thermal performance can be an increased with a larger board size which conflicts with the need to be small and hand-held.
This makes high power design very important. Like in the case of Electromagnetic Interference (EMI), designing for high power applications is a process of making decisions and planning to mitigate problems that may or may not occur.
Surprisingly, poor high-power design does not always result in an electrical fire or smoke. The results are a spectrum. In the case of the electrical fire, the results may be instantaneous, and the first time the motor spins is also the last time the motor spins due to catastrophic board damage. This indicates that something is fundamentally faulty with the design, or some aspects of normal operation are amplified. As a result, some aspect of the design can be reduced or mitigated, controlling the source of damage and reducing its negative effects on the system to bring probability of damage to a negligible level.
In other cases, the motor will spin and damage might occur when commanded to deliver more current, or stop rotating. A change in operation stresses the system beyond what it is capable. In more difficult cases, the motor will spin at the same current or speed for a hundred hours but fail minutes before the test concludes. This could mean that a special use case might cause the design to fail, or regular operation might result in damage to the design over time until a permanent and observed failure occurs.
Understanding the differences in the spectrum allows the designer to understand what kind of change is needed to fix or prevent damage. Just like the spectrum of damage, the spectrum of changes could vary from replacing a component on the bill of materials to a complete redesign of the schematic and layout.
This example covers a hypothetical and uses the principles of high-power design to improve a high-power motor driver application. Note, this example serves to show that how the process is utilized and rest of the application note explains the theory that eventually results in the process used.
Consider the following example:
Examining the givens, there is a fundamental problem with the system. In this context, the functions of the gate drive circuit must be verified as the next step in troubleshooting.
After going through the troubleshooting steps, the notable observations are:
The short between gate-to-source seems to indicate that voltage inductive spiking is the problem as an absolute maximum limit could have been exceeded. This is further supported by the lack of damage at a lower current level. In addition, if there is damage is primarily on a singular phase then this might indicate that the layout is not optimized and might be contributing to the problem.
With a goal to reduce the voltage spiking:
By using an oscilloscope probe on the low-side gate and source voltages at 20 A, the waveforms show there is negative voltage spiking on the low-side source that is close but does not exceed the absolute maximum limits defined in the DRV835x 100-V Three-Phase Smart Gate Driver data sheet.
With some indicators that negative spiking on the low-side source and gate is the problem, some solutions include:
Evaluate the options that may fix the problem. To avoid a redesign of the board, its best to look for a change on the bill of materials or populate components that were previously depopulated.
This application note breaks down the process into a development of troubleshooting guidelines, a library of external circuits, TI driver product features, or layout techniques to combat the volatile nature of higher power systems.