Getting started with embedded metering applications using MSP430i20xx MCUs
Start developing your power or energy measurement with this virtual bundle, and see the required hardware, software, example code, demos and key documentation.
開發板
EVM430-I2040S — 適用於分戶量測的 MSP430I240 評估板
支援產品和硬體
EVM430-I2040S — 適用於分戶量測的 MSP430I240 評估板
版本: null
發行日期:
硬體程式設計工具
MSP-FET — MSP MCU 程式設計工具和偵錯器
支援產品和硬體
MSP-FET — MSP MCU 程式設計工具和偵錯器
版本: null
發行日期:
開發套件
MSP-EXP430F5529LP — MSP430F5529 LaunchPad™ development kit for USB
Jumper wires are required but do not come with this kit.
支援產品和硬體
MSP-EXP430F5529LP — MSP430F5529 LaunchPad™ development kit for USB
版本: null
發行日期:
子卡
MSP-ISO — Isolation Adapter for MSP LaunchPad Development Kits
Jumper wires are required but do not come with this kit.
MSP-ISO — Isolation Adapter for MSP LaunchPad Development Kits
版本: null
發行日期:
應用軟體及架構
MSP430-ENERGY-MEASUREMENT — Energy Measurement Library for MSP430 MCUs with 24-Bit Sigma-Delta ADCs
支援產品和硬體
產品
感測 MCU
硬體開發
子卡
開發套件
開發板
MSP430-ENERGY-MEASUREMENT — Energy Measurement Library for MSP430 MCUs with 24-Bit Sigma-Delta ADCs
版本: 1.40.00.03
發行日期: 2020/7/29
Windows Installer for Energy Measurement Design Center
SHA-256 校驗和
macOS Installer for Energy Measurement Design Center
SHA-256 校驗和
Linux Installer for Energy Measurement Design Center
SHA-256 校驗和
產品
感測 MCU
硬體開發
子卡
開發套件
開發板
文件
Energy Measurement Design Center Technology Guide
Energy Measurement Design Center API Guide
版本資訊
The Energy Measurement Design Center is a rapid development tool that enables energy measurement using TI MSP430i20xx and MSP430F67xx Flash-based microcontrollers (MCUs). It includes a graphical user interface (GUI), documentation, software library and examples that can simplify development and accelerate designs for power monitoring and energy measurement in smart grid and building automation applications. Start by dragging and dropping a MCU, voltage sensors, and current sensors into the GUI workspace. Configure the MCU and each sensor according to your system configuration. The GUI will check for errors before generating the source code. Import the code into an IDE and program the MCU. The GUI will allow you to easily calibrate the device and view the results.
新功能
- Software
- Fixed an issue where the MSP430i20xx OSR (sampling rate) did not change from the default value.
- Removed duplicate hal_system_Init() call.
- Re-initialized results after disabling interrupts and writing calibration factors to INFO memory.
- Re-calibrated MSP430i20xx EMDC example projects and firmware images.
- Technology Guide
- Included a flowchart for the EMDC application code including foreground and background processes.
- Added a Known Limitations section to the Introduction for more awareness.
- Fixed the Result Parameter command values in the Commands from Target to EMDC section and sequence diagrams.
- Added more details about the packet structure and checksum calculation in the Communication Protocol Spec section.
- Included the default UART communication settings.
- Updated the EMDC start-up image to fix a broken pixel in the platform bar.
- Fixed some minor formatting issues.
軟體程式設計工具
UNIFLASH — UniFlash for most TI microcontrollers (MCUs) and mmWave sensors
支援產品和硬體
產品
Low-power MCUs
Wi-Fi 產品
即時數位電源 MCU
即時馬達控制與自動化 MCU
多媒體與工業網路 SoC
工業 mmWave 雷達感測器
汽車 mmWave 雷達感測器
汽車動力系統、區域和底盤控制 MCU
汽車車身和照明 MCU
通用型 MCU
音訊與雷達 DSP SoC
UNIFLASH — UniFlash for most TI microcontrollers (MCUs) and mmWave sensors
版本: 9.4.1
發行日期: 2026/1/19
SHA-256 校驗和
SHA-256 校驗和
SHA-256 校驗和
產品
Low-power MCUs
Wi-Fi 產品
即時數位電源 MCU
即時馬達控制與自動化 MCU
多媒體與工業網路 SoC
工業 mmWave 雷達感測器
汽車 mmWave 雷達感測器
汽車動力系統、區域和底盤控制 MCU
汽車車身和照明 MCU
通用型 MCU
音訊與雷達 DSP SoC
版本資訊
CCStudio UniFlash is a standalone tool used to program on-chip and external flash memory on TI MCUs and on-board flash memory for Sitara processors. UniFlash has a GUI, command line, and scripting interface. UniFlash is available free of charge.
新功能
- Fixed issue with Program Verification feature, where certain programs were passing verification incorrectly
- Fixed issue with C2000 16-bit Checksum feature to support file paths that include spaces