SBAA274A September 2018 – March 2023 ADS1118 , ADS1119 , ADS1120 , ADS112C04 , ADS112U04 , ADS1146 , ADS1147 , ADS1148 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS125H02 , ADS1260 , ADS1261 , ADS1262 , ADS1263
The measurement circuit requires:
Another feature of many precision ADCs is an internal reference. The internal reference is often used as only the ADC reference. However, if the reference is buffered and brought out of the device to a pin, it can be used to bias a thermocouple. While this reference voltage may not be at exactly the mid-supply voltage, it is likely in the input range of the PGA. Consult the ADC data sheet for specific PGA common-mode and absolute input ranges.
First, enable the internal reference voltage. The REFOUT line is then attached to the thermocouple negative input, while a resistor is used to pull up the thermocouple positive input to AVDD. As in the similar design using VBIAS, the large pullup resistor is used for burn-out detection. If the thermocouple has burned out and become high impedance, the ADC over-ranges and gives a full-scale reading.
A single pullup resistor may be attached to the positive thermocouple lead for burn-out detection. In the case of a burned-out thermocouple, the negative lead is still set to mid-supply, while the positive lead is pulled up to AVDD. As in the previous designs, the pullup resistor is generally large to keep the bias current low. Any bias current reacting with the lead resistance of the thermocouple becomes an error in the measurement. However, the biasing current must be large enough to overcome the ADC input current. If a burn-out condition exists, the pullup resistor must be able pull the positive analog input high enough above VBIAS to give an ADC full-scale reading (7FFFh, assuming a 16-bit bipolar ADC).
As in the previous topologies, the biasing resistor must be high to keep the bias current low. Bias current reacting with the resistive leads of the thermocouple is measured as an error voltage. Also, the ADC input current reacts with the series input filter resistance and multiplexer resistance to add another measurement error.
Unless the cold junction is at 0°C, there should be a separate cold-junction measurement. This measurement can be done through several different methods, using either an RTD, calibrated thermistor, or a variety of integrated circuit temperature sensors.