Figure 2-1 to Figure 2-3 show the schemes of power designs with second stage filter, correspond to the
power designs with first stage sense, second stage sense and hybrid sense. The
advantages and disadvantages of each design are summarized in the following:
- With first stage sense, the feedback sense point is Vo1 and the
voltage drop on DCR of L2 can’t be compensated, so load regulation
performance is worse. But the stability is good as the double poles of second
stage filter are not included in the control loop.
- With second stage sense, the voltage drop on DCR of L2 can be
compensated. But the double poles of second stage filter can have obvious
impacts on the loop response. When the values of L2 and C2
become larger, the double poles frequency of second stage filter reduces and can
be closer to bandwidth, which can cause less phase margin and possible
instability. That limits the maximum value of second stage filter components
selection and the ability to reduce output ripple.
- With hybrid sense, the feed-forward capacitor Cff is connected with
Vo1 and upper feedback resistor R1 is connected with
Vo2. The AC disturbance of Vo1 can be coupled to
VFB and reduce the portion of Vo2 AC disturbance in
total feedback. That can help to reduce the effects of second stage filter on
loop stability. And the load regulation performance is also good since the DC
regulation is based on feedback from Vo2. So the loop stability and
output accuracy can be made sure at the same time with the hybrid feedback
sense.
Due to the obvious advantages of
hybrid sense, the application design method in this application note is based on
this sense approach.