SLUAAJ0 February 2024 TPS51397A , TPS54308 , TPS54320 , TPS54350 , TPS54538 , TPS54620 , TPS54622 , TPS54821 , TPS54824 , TPS563300 , TPS566231 , TPS566235 , TPS566238 , TPS568230 , TPS56C215 , TPS62933 , TPS62933F , TPS62933O
To make sure of the system stability margin, the recommendation is that the loop gain needs to cross 0dB with -20dB/dec slope. By adjusting the frequencies of those poles and zeros shown in Figure 5-3, there can be many different approaches to achieve the target. This application note only proposes one simplified stability design method as reference.
In the stability design of normal PCM buck converter without 2nd stage filter, it’s recommended to make fZ-EA smaller than bandwidth fcross and keep the fP-ci & fP2-EA larger than bandwidth, which can make loop gain cross 0dB with -20dB/dec slope [5-6]. Those design limitations are inherited in this design method.
If the zero Zff is inside bandwidth, it can further increase converter bandwidth fcross and improve dynamic response. But that would make it more difficult to estimate the bandwidth and cause more uncertainties. To simplify the stability design, fZff>fcross is given as a restriction. Typically, the bandwidth of PCM converter is set as fcross≤fSW/10.
Since the expression of fZff in Equation 23 is very complicated, an example of how to use Microsoft® Excel® or MATLAB® to calculate fZff is introduced in Appendix A.
Recommend to keep fP-2nd > 2 x fcross to avoid effects of the conjugate poles on phase margin. Combined with Equation 22, the range of the 2nd stage filter capacitor C2 can be derived as:
The bandwidth fcross with 2nd stage filter can be received with Equation 25.
For specific device TPS62933F, the bandwidth fcross is:
As mentioned in section 5, the conjugate zeros Z2nd are located in the right half plane with negative damping, if considering L2 as an designed for inductor with no DCR.
The same effect for lack of damping also exists on the conjugate poles P2nd. Those effects can cause resonance peak and loop gain may crosses 0dB twice, as shown in the case DCRL2=0 of Figure 6-1.
The second gain crossing has a chance to cause system instability [7]. Like the example in Figure 6-1, increasing DCRL2 can effectively reduce the resonance peak amplitude and avoid second gain crossing. Increasing conjugate poles frequency fP-2nd is another approach to avoid second gain crossing, like shown in Figure 6-2.
As second gain crossing does not normally happen with DCRL2 of real inductor or ferrite bead (several mΩ or larger), further mathematical analysis is not included in this application note. But the above two methods can be tried, if you already follow the design flow in next section, but there is still instability issue.