SWRA670A April 2020 – October 2022 CC1350 , CC1352P , CC1352R , CC2400 , CC2420 , CC2430 , CC2500 , CC2520 , CC2530 , CC2538 , CC2540 , CC2541 , CC2543 , CC2544 , CC2545 , CC2564 , CC2590 , CC2591 , CC2592 , CC2620 , CC2630 , CC2640 , CC2650 , CC2652P , CC2652R , CC2652R7 , CC2652RSIP , CC3100 , CC3120 , CC3135 , CC3135MOD , CC3200 , CC3200MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF , WL1801MOD , WL1805MOD , WL1807MOD , WL1831
The performance criteria are used to take a decision on whether a radio equipment passes or fails immunity tests. The performance criteria are:
The equipment should meet the minimum performance criteria as specified in the following Table 7-3 and Table 7-4.
Criteria | During test | After test (or as a result of the application of the test) |
---|---|---|
A | should operate as intended.(1) | should operate as intended. |
B | May be loss of function. | Functions should be self-recoverable. |
C | May be loss of function. | Functions should be recoverable by the operator. |
Phenomenon | Performance Criteria |
---|---|
CT (Continuous phenomenon applied to Transmitters) | Criteria A should apply (see Table 7-3) Tests should be repeated with the EUT in standby mode (if applicable) to ensure that unintentional transmission does not occur. In systems using acknowledgement signals, it is recognized that an ACKnowledgement (ACK) or Not ACKnowledgement (NACK) transmission may occur, and steps should be taken to ensure that any transmission resulting from the application of the test is correctly interpreted. |
CR (Continuous phenomenon applied to Receivers) | Criteria A should apply (see Table 7-3) Where the EUT is a transceiver, under no circumstances, should the transmitter operate unintentionally during the test. In systems using acknowledgement signals, it is recognized that an ACK or NACK transmission may occur, and steps should be taken to ensure that any transmission resulting from the application of the test is correctly interpreted. |
TT (Transient phenomenon applied to Transmitters) | Criteria B should apply, except for voltage dips of 100 ms and voltage interruptions of 5000 ms duration, for which performance criteria C should apply (see Table 7-3) Tests should be repeated with the EUT in standby mode (if applicable) to ensure that unintentional transmission does not occur. In systems using acknowledgement signals, it is recognized that an ACKnowledgement (ACK) or Not ACKnowledgement (NACK) transmission may occur, and steps should be taken to ensure that any transmission resulting from the application of the test is correctly interpreted. |
TR (Transient phenomenon applied to Receivers) | Criteria B should apply, except for voltage dips of 100 ms and voltage interruptions of 5000 ms duration, for which performance criteria C should apply (see Table 7-3) Where the EUT is a transceiver, under no circumstances, should the transmitter operate unintentionally during the test. In systems using acknowledgement signals, it is recognized that an ACK or NACK transmission may occur, and steps should be taken to ensure that any transmission resulting from the application of the test is correctly interpreted. |