DLPA068C November 2019 – May 2022 DLP160AP , DLP160CP , DLP2000 , DLP2010 , DLP230NP , DLP3010 , DLP3310 , DLP470NE , DLP470TE , DLP4710 , DLP471NE , DLP471TE , DLP471TP , DLP472NE , DLP472TE , DLP480RE , DLP550HE , DLP550JE , DLP650LE , DLP650NE , DLP650TE , DLP651LE , DLP651NE , DLP660TE , DLP670RE , DLP780NE , DLP780TE , DLP781NE , DLP781TE , DLP800RE , DLP801RE , DLP801XE , DLPA1000 , DLPA2000 , DLPA2005 , DLPA3000 , DLPA3005 , DLPC2607 , DLPC3420 , DLPC3421 , DLPC3430 , DLPC3433 , DLPC3435 , DLPC3438 , DLPC3439 , DLPC6401
DLP® is a registered trademark of Texas Instruments.
All trademarks are the property of their respective owners.
Brightness requirements are one of the key considerations to account for when designing any projection system.
The terms projector brightness and image brightness are used throughout this paper. Here is how they are defined for the sake of this paper:
The term projector can often have limiting connotations. Classically, a projector is a system used only to display a video or image on a wall, and while this is still the case, projection systems can be utilized to display any form of visuals or infographics on virtually any display surface. These can be used for smart home displays, digital signage, laser TVs, and many other potential applications. DLP technology enables projection systems of many sizes for use in countless applications, in addition to supporting bright, vivid displays for classically defined projectors.
The two of the most frequently asked questions from customers who are new to TI DLP technology are: “How much brightness is needed for my application,” and “how bright can the projection system get?” In other words:
The first question is often asked by product developers for whom image quality is the highest priority, whereas the second question is often asked by product developers who have certain technical constraints, most frequently power, size, and cost, which will ultimately constrain the maximum brightness of the projection system.