SLUAAI3 January 2022 TPS62810-Q1 , TPS62811-Q1 , TPS62812-Q1 , TPS62813-Q1 , TPS62816-Q1 , TPS628501 , TPS628501-Q1 , TPS628502 , TPS628502-Q1 , TPS628503 , TPS628503-Q1 , TPS628510 , TPS628511 , TPS628512 , TPS62870 , TPS62870-Q1 , TPS62871 , TPS62871-Q1 , TPS62872 , TPS62872-Q1 , TPS62873 , TPS62873-Q1 , TPS62874-Q1 , TPS62875-Q1 , TPS62876-Q1 , TPS62877-Q1 , TPS62A01 , TPS62A01A , TPS62A02 , TPS62A02A , TPS62A06 , TPS62A06A , TPSM82810 , TPSM82813 , TPSM8287A06 , TPSM8287A10 , TPSM8287A12 , TPSM8287A15 , TPSM8287B30
All trademarks are the property of their respective owners.
Especially for DC-DC converters, meeting a low PDN Impedance is important to reduce the voltage variations due to strict load transient requirements. An ideal PDN design enables a DC-DC converter to supply a stable voltage to a load and maintain it within narrow margins. When designing a PDN, it is important to validate that the output impedance (or input impedance) of a DC-DC converter is meeting its target impedance and achieve low impedance value in the milliohm range. A PDN impedance analysis shows an overlay of the passive component impedances constituting the power network over frequency.
This application report describes a measurement method to evaluate the PDNs of a DC-DC converter, the 2-port shunt-through measurement. This method allows PDN designers to measure down to milliohm impedances while supporting measurement at very high frequencies.
Figure 2-1 shows the 2-Port Shunt-Through circuit configuration to measure impedance. First of all, the S-parameter is calculated to derive the impedance value. As per definition, is:
Assuming that = 50 Ω and << 1 (for very small impedance / resistances - << ) when solving for , the result is:
It is important to note that the measure of is influenced by the VNA performance such as the dynamic range, the signal-to-noise ratio and the effective number of bits.
As all grounds in a VNA refer to the same point, an additional common mode current is created and affects measurement accuracy resulting in measurement errors. A Semi-floating differential amplifier is then used as a ground isolator to minimize ground loop currents.
Figure 2-2 shows a 2-port shunt-through measurement setup. The 2-port shunt-through measurement uses a vector network analyzer (VNA) to compute impedances at very high frequency and a semi-floating differential amplifier to measure impedances down to 1 mΩ. Selecting a semi-floating differential amplifier with a large resistance to common mode current is paramount to improve the accuracy of the measurements especially at lower frequencies.