SLOU583A September 2024 – November 2024 OPT101 , OPT3001 , OPT3001-Q1 , OPT3002 , OPT3004 , OPT3005 , OPT3006 , OPT3007 , OPT4001 , OPT4001-Q1 , OPT4003-Q1 , OPT4041 , OPT4048 , OPT4060
This user’s guide describes the characteristics, operation, and use of the light source evaluation module (LIGHTSOURCE01EVM). This user's guide details how to set up the light source including mounting of the light source and requirements for performing calibration such as creating a dark enclosure to block outside light. The guide also covers how to operate the light source including installation of the provided control software and serial command structure for using the light source with custom automation routines. Throughout this document, the terms evaluation board, evaluation module, and EVM are synonymous with the light source EVM (LIGHTSOURCE01EVM). This document also includes the mechanical drawings and parts list for the EVM.