SNOAA04A March 2020 – June 2021 FDC1004 , FDC1004-Q1 , FDC2112 , FDC2112-Q1 , FDC2114 , FDC2114-Q1 , FDC2212 , FDC2212-Q1 , FDC2214 , FDC2214-Q1 , LDC0851 , LDC1041 , LDC1051 , LDC1101 , LDC1312 , LDC1312-Q1 , LDC1314 , LDC1314-Q1 , LDC1612 , LDC1612-Q1 , LDC1614 , LDC1614-Q1 , LDC2112 , LDC2114 , LDC3114 , LDC3114-Q1
Simulation tools similar to SPICE are an important part of the design process for many systems because they reveal design problems before prototypes are built. SPICE, however, is not suitable to simulate inductive sensing systems because it does not include target interactions with the sensor coil. The open-source magnetics simulation software FEMM (Finite Element Method Magnetics) can provide information about these target interactions and the robustness of the system before production. Before using FEMM, we recommend using the LDC Tools Excel calculator to design the sensor coil, as well as reading LDC Sensor Design and LDC Target Design. For smooth targets that are at least as large as the sensor coil, TI also recommends using the Excel_FEMM tool (included in LDC Tools), which will automatically simulate custom sensors in FEMM. For smaller or irregularly shaped targets, the following guide will give the reader working knowledge of FEMM for inductive sensing simulations. The program can be downloaded from the FEMM home page.