SLVA505A February 2012 – July 2024 DRV8800 , DRV8801 , DRV8802 , DRV8803 , DRV8804 , DRV8805 , DRV8806 , DRV8811 , DRV8812 , DRV8813 , DRV8814 , DRV8818 , DRV8821 , DRV8823 , DRV8824 , DRV8828 , DRV8829 , DRV8830 , DRV8832 , DRV8832-Q1 , DRV8833 , DRV8834 , DRV8835 , DRV8836 , DRV8837 , DRV8840 , DRV8841 , DRV8842 , DRV8843 , DRV8844 , DRV8870 , DRV8871 , DRV8872
There is much misunderstanding about the current ratings used with motor driver ICs, especially as related to the selection of a motor driver part for a specific application. Complicating matters further is that there is no standard way of specifying current ratings, so the exact meaning of the ratings can differ from one vendor to another and in some cases even between different parts from the same vendor. This application note explains the meaning of the different current ratings applied to motor driver parts and specifically explains the ratings found in TI motor driver device data sheets.
PowerPAD™ is a trademark of Texas Instruments.
All trademarks are the property of their respective owners.