Selecting the Create Design tool displays
the simulation environment (Figure 3-1).
A
3D model of the system is displayed and updated as
user entry fields are changed. The Create
Design page contains several key interface
selections.
- Simulation Name: Selecting the pencil icon
allows users to change the name of the simulation.
This is the name displayed on the home screen tile
under My Designs.
- Save: Selecting this overwrites any existing configuration settings for the
design. Any changes made to an existing design without selecting Save are lost when
exiting the simulation environment.
- Import and Export Menu: This menu includes
options to externally save simulation information
contained in the tool (Figure 3-2).
- Save As: This selection allows users to create a new saved design in My
Designs after being prompted for a new design name.
- Export Input Parameters to JSON: This creates a local file which can be
imported by any user.
- Export Report to CSV: This exports all data and settings into a single .csv
file after running a simulation. This file is formatted for use with pivot tables and
similar data processing tools after running a simulation. This is particularly
powerful when analyzing data from parameterized sweeps.
- Export Report to PDF: This generates a PDF report showing the simulation
setup, input plots, output plots, and tabulated simulation data.
- Import Input Parameters from JSON: This loads simulation local files
exported with the Export Input Parameters to JSON function.
- Simulation Mode: These tabs allow the user to change between three simulation
modes.
- Design: This is the standard
design format.
- Parametric Sweep: Parametric
sweep allows for user input fields to be stepped through either ranges or discrete
values to compare the impact of system tolerances on end behavior. This is discussed
in detail in Section 6.
- Compare Designs: This runs a
comparison between two simulations side by side after multiple designs of the same
type have been saved. This is discussed in detail in Section 7.
- 3D Render: The 3D model of the system can be adjusted freely to observe the
motion of the magnet relative to the sensors. The tool does not prevent collisions and the
user is responsible for placing the devices appropriately. The following list of functions
help users navigate in the tool.
- Click and Drag: This changes the
camera perspective.
- Scroll Wheel: This zooms in or out
from the design center of focus.
- Shift + Click and Drag: This pans the
camera and adjusts the center of focus.
- Cartesian Coordinates: The axes are colored following this convention.
X = red
Y = green
Z = blue
Selected on this marker quickly
auto-aligns the view to the direction of the specific axis selected.
- Simulation Input Fields: These menu feature allows users to customize the
simulation settings. The various fields are explained in Section 4.2.
For help understanding magnet and
sensor rotation within the simulation environment please refer to Section A.3.
- Simulate: Selecting this button runs the
simulation and generates field data and output
results.