The user interface displays the
results after simulating a particular setup. This page has several points for the
user to interact with (Figure 5-1).
- Edit Design: Click the
Edit Design tab to return to the simulation input panel.
- Simulation Environment:
Navigate this feature as described in Section 3.
- Play: Select this button
to play an animation of the magnet motion. The progress slider can be clicked
and dragged to set the animation to a specific frame. Watching the full
animation is helpful to verify the input parameters related to magnet motion are
correct and match expectations. This is particularly useful in cases where the
magnet is rotated.
- Sensor Select: Select this
option for simulations with more than one sensor to switch the field and output
results to display the simulation results for the selected sensor.
- Die Select: Select this
feature to display the results for the selected die in devices with more than
one die.
- Magnet Field Density Versus
Distance: This plot displays Magnetic Flux Density in millitesla
versus the travel of the magnet. This plot demonstrates the sensor orientation
and not the global coordinate space. The field is calculated based on the
alignment shown in Appendix A if the sensor is rotated.
- Single click the trace in
the legend to remove individual results in the plot from view.
- Double click the trace in
the legend to keep all results from view in the plot except selected
results.
- Hovering over any trace
with the selection tool shows the value of the field at that point.
- Use the selection tool
scroll wheel to zoom in on the plot.
- Select the home icon to
return to the full view of the plot.
-
Click the double arrow
icon in the top right of the panel to create an enlarged pop-out of
the graph.
- Device Output - Emulated
device outputs are overlaid in the device output plots. Outputs of the same type
are overlaid on a single graph. This plot can be manipulated using the same
controls as the input magnetic field plot.
- Scroll Bar - Using the
mouse scroll wheel over the plot zooms the plot instead of advancing to the next
plot. Some devices have more than one output mode. When this scroll bar is
present there is another plot available by scrolling down.
- Input Parameters - This
tab expands and collapses to show the parameters used for the simulation. This
is helpful for allowing the user to remain on the simulation outputs page
without needing to navigate to Edit Design, which removes the output
results from view.