SBAA532A February 2022 – March 2024 ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS130E08 , ADS131A02 , ADS131A04 , ADS131E04 , ADS131E06 , ADS131E08 , ADS131E08S , ADS131M02 , ADS131M03 , ADS131M04 , ADS131M06 , ADS131M08
Many precision sensors are formed from a Wheatstone bridge circuit configuration. This circuit configuration enables accurate differential measurements for resistive elements. These elements can be used to measure weight, pressure, temperature, and a variety of other types of sensor parameters. Achieving the most accurate bridge measurements with precision analog-to-digital converters (ADCs) requires a detailed understanding of how these sensors work, how they are calibrated, how they connect to an ADC, and how the ADC is configured. This application note presents an overview of the bridge circuit, how bridges are used to measure different forces, how the ADC measurement is set up, and what errors can arise in the measurement. This application note starts with an overview of bridge circuit basics, how they are constructed, and what parameters are important when designing a bridge measurement system. Circuits are presented showing connections to precision ADCs.
All trademarks are the property of their respective owners.
A Wheatstone bridge is a circuit used to measure a change in resistance among a set of resistive elements. The circuit has two parallel resistive branches that act as voltage dividers for the excitation voltage, VEXCITATION. The output of each resistor divider is nominally at VEXCITATION divided by two. With no applied load, the change in the resistance of the elements, ΔR, is equal to zero. Assuming an ideal system where the nominal resistance of each element is R, each voltage divider is at the same potential and the differential bridge output voltage, VOUT, is zero. When a load is applied, one or more of the elements changes resistance such that ΔR ≠ 0 Ω. This causes a change in VOUT that can be calculated very precisely by making a differential measurement across the bridge. Figure 1-1 shows the basic configuration of a simple bridge circuit using resistive elements.
The basic bridge circuit is constructed using resistive elements with a single variable element in the bridge. This element is a resistive transducer that translates some physical parameter into a change in resistance. If this change in resistance is proportional to a change in the physical parameter, measuring ΔR yields an accurate representation of the physical property being sensed. While this document focuses on bridges using resistive elements, it is possible to construct a bridge using inductive or capacitive elements as well.
Bridge operation can be better understood by analyzing each side of the bridge in more detail. For example, the right side of the bridge in Figure 1-1 looks like the voltage divider circuit shown in Figure 1-2:
Equation 1 calculates VOUT with respect to ground for the system in Figure 1-2:
Assuming VEXCITATION = 6 V, R = 3000 Ω, and ΔR = 3 Ω, Equation 1 can be used to calculate that VOUT = 3.0015 V. Then, the voltage across R is calculated to be VR = VEXCITATION - VOUT = 2.9985 V. This yields a voltage across ΔR of VΔR = VOUT - VR = 0.003 V. While Equation 1 works in theory to calculate VOUT, VR, and VΔR, a real system must measure VOUT and VR to be able to derive VΔR. This can introduce additional challenges due to the limitations of standard measurement equipment.
For example, a simple 4-digit multimeter used to measure VOUT and VR could produce rounding errors that affect the calculation of VΔR: if the multimeter rounds VOUT = 3.0015 V up to 3.002 V and VR = 2.9985 V down to 2.998 V, then VΔR = 0.004 V; or, if VOUT is rounded down to 3.001 V and VR is rounded up to 2.999 V, then VΔR = 0.002 V. Both of these cases yield a measurement error of 1 mV relative to a 3-mV signal, or ±33% error. Ultimately, the 4-digit multimeter does not have enough resolution to consistently determine the precise value of ΔR by measuring across either resistive element in the divider.
For better results, the single-ended measurement shown in Figure 1-2 is changed to a differential measurement by placing the resistive transducer in a bridge configuration. In Figure 1-3, the bridge uses a second resistive path in parallel with the transducer path. With no applied load, ΔR = 0 Ω and VOUT = 0 V.
Equation 2 calculates the differential output voltage for the system shown in Figure 1-3 assuming R1 = R2 = R3 = R and R4 = R + ΔR.
Using the same values from the single-ended example where VEXCITATION = 6 V, R = 3000 Ω, and ΔR = 3Ω, VOUT is now calculated to be 1.49925 mV. Importantly, the same 4-digit multimeter can measure VOUT much more precisely and on a millivolt scale as either 1.499 mV (rounded down) or 1.500 mV (rounded up). Measuring VOUT differentially in a bridge configuration yields a measurement error of <1 μV relative to a 1.5-mV signal, or 0.067%. This result occurs because a bridge configuration enables direct measurement of ΔR instead of a comparative measurement between ΔR and R. A direct measurement also enables VOUT to be amplified to get a larger input signal to the ADC. This amplification enables higher-resolution measurements of smaller values of ΔR.
One challenge with a single active resistive element bridge is that it has an inherent non-linearity in the measurement. Different bridge constructions have different non-linearities, and some topologies eliminate this inherent non-linearity. This is discussed in more detail in the next section.