SBAA532A February 2022 – March 2024 ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS130E08 , ADS131A02 , ADS131A04 , ADS131E04 , ADS131E06 , ADS131E08 , ADS131E08S , ADS131M02 , ADS131M03 , ADS131M04 , ADS131M06 , ADS131M08
The final bridge configuration is constructed with four active elements that each have the same magnitude change in resistance for the same strain. However, this change is in opposite directions on opposite sides of the bridge. This configuration is known as a full bridge, and is shown in Figure 2-8.
Equation 12 and Equation 13 calculate VOUT for the bridge with four active elements shown in Figure 2-8:
Similar to all of the previous bridge configurations, VOUT is proportional to VEXCITATION and ΔR if ΔR is small. The benefit of a four-active-element bridge is that the sensitivity is two times greater than both two-active-element bridge configurations and four times greater than the single-active-element bridge. Moreover, a four-active-element bridge topology has no inherent non-linearity in the bridge output. This is true for both voltage and current excitation.