SBAA532A February 2022 – March 2024 ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS130E08 , ADS131A02 , ADS131A04 , ADS131E04 , ADS131E06 , ADS131E08 , ADS131E08S , ADS131M02 , ADS131M03 , ADS131M04 , ADS131M06 , ADS131M08
It is possible to reduce the non-linearity in a bridge with one active element by using current excitation instead of voltage excitation, as shown in Figure 2-4.
Equation 5 calculates the resulting output voltage, VOUT, when IEXCITATION splits between each branch of the bridge in Figure 2-4:
Converting and collecting like terms, Equation 5 simplifies to Equation 6:
Comparing the denominators for Equation 6 (4 ∙ R + ΔR) and Equation 4 (2 ∙ R + ΔR) reveals that the non-linearity error due to the topology of a one-active-element bridge using current excitation is reduced by approximately ½ relative to the same circuit using voltage excitation.
A bridge measurement system using current excitation has additional benefits and challenges. See Section 6.5 for more information about how this circuit is implemented.