SLUAAO2 March   2023 CSD13201W10 , CSD13202Q2 , CSD13302W , CSD13303W1015 , CSD13306W , CSD13380F3 , CSD13381F4 , CSD13383F4 , CSD13385F5 , CSD15380F3 , CSD15571Q2 , CSD16301Q2 , CSD16321Q5 , CSD16322Q5 , CSD16323Q3 , CSD16325Q5 , CSD16327Q3 , CSD16340Q3 , CSD16342Q5A , CSD16401Q5 , CSD16403Q5A , CSD16404Q5A , CSD16406Q3 , CSD16407Q5 , CSD16408Q5 , CSD16409Q3 , CSD16410Q5A , CSD16411Q3 , CSD16412Q5A , CSD16413Q5A , CSD16414Q5 , CSD16415Q5 , CSD16556Q5B , CSD16570Q5B , CSD17301Q5A , CSD17302Q5A , CSD17303Q5 , CSD17304Q3 , CSD17305Q5A , CSD17306Q5A , CSD17307Q5A , CSD17308Q3 , CSD17309Q3 , CSD17310Q5A , CSD17311Q5 , CSD17312Q5 , CSD17313Q2 , CSD17318Q2 , CSD17322Q5A , CSD17327Q5A , CSD17381F4 , CSD17382F4 , CSD17483F4 , CSD17484F4 , CSD17501Q5A , CSD17505Q5A , CSD17506Q5A , CSD17507Q5A , CSD17510Q5A , CSD17522Q5A , CSD17527Q5A , CSD17551Q3A , CSD17551Q5A , CSD17552Q3A , CSD17552Q5A , CSD17553Q5A , CSD17555Q5A , CSD17556Q5B , CSD17559Q5 , CSD17570Q5B , CSD17571Q2 , CSD17573Q5B , CSD17575Q3 , CSD17576Q5B , CSD17577Q3A , CSD17577Q5A , CSD17578Q3A , CSD17578Q5A , CSD17579Q3A , CSD17579Q5A , CSD17581Q3A , CSD17581Q5A , CSD17585F5 , CSD18501Q5A , CSD18502KCS , CSD18502Q5B , CSD18503KCS , CSD18503Q5A , CSD18504KCS , CSD18504Q5A , CSD18509Q5B , CSD18510KCS , CSD18510KTT , CSD18510Q5B , CSD18511KCS , CSD18511KTT , CSD18511Q5A , CSD18512Q5B , CSD18513Q5A , CSD18514Q5A , CSD18531Q5A , CSD18532KCS , CSD18532NQ5B , CSD18532Q5B , CSD18533KCS , CSD18533Q5A , CSD18534KCS , CSD18534Q5A , CSD18535KCS , CSD18535KTT , CSD18536KCS , CSD18536KTT , CSD18537NKCS , CSD18537NQ5A , CSD18540Q5B , CSD18541F5 , CSD18542KCS , CSD18542KTT , CSD18543Q3A , CSD18563Q5A , CSD19501KCS , CSD19502Q5B , CSD19503KCS , CSD19505KCS , CSD19505KTT , CSD19506KCS , CSD19506KTT , CSD19531KCS , CSD19531Q5A , CSD19532KTT , CSD19532Q5B , CSD19533KCS , CSD19533Q5A , CSD19534KCS , CSD19534Q5A , CSD19535KCS , CSD19535KTT , CSD19536KCS , CSD19536KTT , CSD19537Q3 , CSD19538Q2 , CSD19538Q3A , CSD22202W15 , CSD22204W , CSD22205L , CSD22206W , CSD23202W10 , CSD23203W , CSD23280F3 , CSD23285F5 , CSD23381F4 , CSD23382F4 , CSD25202W15 , CSD25211W1015 , CSD25213W10 , CSD25304W1015 , CSD25310Q2 , CSD25402Q3A , CSD25404Q3 , CSD25480F3 , CSD25481F4 , CSD25483F4 , CSD25484F4 , CSD25485F5 , CSD25501F3 , CSD75207W15 , CSD75208W1015 , CSD83325L , CSD85301Q2 , CSD85302L , CSD85312Q3E , CSD86311W1723 , CSD87312Q3E , CSD87313DMS , CSD87501L , CSD87502Q2 , CSD87503Q3E , CSD88537ND , CSD88539ND

 

  1.   Abstract
  2.   Trademarks
  3. 1Using MOSFET Safe Operating Area Curves in Your Design
  4. 2Review the SOA Graph
  5. 3Applications Where SOA is Important
  6. 4Using the Data Sheet SOA Graph
  7. 5Temperature Derating of SOA
  8. 6Estimating SOA for Different Pulse Widths
  9. 7Estimating SOA for Non-Square Waveforms
  10. 8Summary
  11. 9References

Estimating SOA for Non-Square Waveforms

What if the waveforms are not square? TI performs SOA testing to destruction using square waveforms as shown in Figure 7-1.

GUID-20230301-SS0I-BFFM-QGVN-6JQSCMDL5T88-low.png Figure 7-1 Typical SOA Test Waveform

In section 2.3.3 of the above mentioned application report, Robust Hot Swap Design, a method is presented for approximating the MOSFET stress as a square pulse with equivalent energy and pulse width as follows:

Equation 11. E1=E2=0t1vDSt×iDStdt
Equation 12. t2=E2PMAX

In many applications, one of the waveforms is a linear ramp while the other is held constant. For example, in a hot swap circuit during inrush, VDS is ramping down while IDS is constant as shown in Figure 7-2.

Figure 7-2 Hot Swap Inrush Example Waveform

For this example, assume VDS decays linearly from 12 V down to 0 V in 20 ms while IDS = 6 A. The energy, E1, in the pink shaded area under the power curve is calculated as follows:

Equation 13. E1=0t1vDSt×iDStdt
Equation 14. vDSt=VDS×1-tt1
Equation 15. iDSt=IDS
Equation 16. E1=VDS×IDS0t11-tt1dt=VDS×IDS×t12

For the equivalent square pulse, the energy in the blue shaded area is assumed to be equal and the power P2 is the same as the maximum power in the non-square pulse.

Equation 17. E1=E2=PMAX×t2
Equation 18. t2=E2PMAX=VDS×IDS×t12VDS×IDS=t12

Inserting the values from the example:

Equation 19. VDS=12 V
Equation 20. IDS=6 A
Equation 21. t1=20 ms
Equation 22. PMAX=VDS×IDS=12 V×6 A=72 W
Equation 23. t2=t12=20 ms2=10 ms

Next, go back and confirm that the equivalent square pulse, VDS = 12 V and IDS = 6 A is below the 10 ms curve on the CSD17570Q5B SOA curve as shown in Figure 7-3.

Figure 7-3 SOA Inrush Example

This methodology can be extended for use with other types of pulses including non-monotonic, exponential, constant power, and so on.