SLVAE36A September 2018 – July 2021 LM43600 , LM43601 , LM46001 , LM46002 , LM5160A , LM5161 , LM5165 , LM5166 , LM61460-Q1 , LM73605 , LM73605-Q1 , LM73606-Q1 , LM76003 , LMR33620 , LMR33630 , LMR36006 , LMR36015 , LMR36500 , LMR36501 , LMR36502 , LMR36503 , LMR36506 , LMZ36002 , LMZM23600 , LMZM23601 , LMZM33602 , LMZM33603 , LMZM33606 , TPS54218 , TPS54360B , TPS54418 , TPS54424 , TPS54560B , TPS54618 , TPS55010 , TPS62148 , TPS62821 , TPS62822 , TPS62823 , TPS82130 , TPS82140 , TPS82150 , TPSM365R15 , TPSM365R3 , TPSM365R6
Webench is a registered trademark of Texas Instruments.
All trademarks are the property of their respective owners.
PLCs benefit from a DC/DC point of load power solution that supports the needs of advanced analog and digital integrated circuits, offers high efficiency with good thermal performance, and reduces the overall component count and cost. Point of load strategies can vary, but PLCs are usually provided a 24-VDC input supply from the power supply or occasionally a 12-VDC input. However, the line voltage is susceptible to input voltage transients that originate from motors or relays, causing excessive voltage spike which can damage the system. Voltage spikes also come from power transmission wires routed longer distances introducing parasitic inductance loops causing problems to the DC/DC converters. It is good design practice to account for unpredictable voltage spikes by choosing a DC/DC converter that withstands an additional 50% voltage rating, or 36 V, from a 24-V rail if no other line voltage conditioning exists in the system.
In almost all cases, 5-V and 3.3-V rails are used as secondary regulation rails from 24-V or 12-V source to power low-voltage sub-systems. Since newer microcontrollers, FPGAs, memory ICs, clocks, and AFEs operate with lower voltages, it is difficult to regulate a 1-V rail with a 24-V input while switching at a higher frequency, such as 1 MHz or above, to maintain a small form factor. As shown in Equation 1, to regulate 1 V from a 24-V input (4.2% duty cycle), the minimum controllable on time of the DC/DC converter must be lower than 40 ns when switching at 1 MHz to avoid noisy pulse-skipping.
Line transients can come from motors and relays in the system, and can cause an excessive voltage spike on the input voltage line. Voltage spikes can also come from power rails or signal transmission lines that are routed longer distances causing problems to the DC/DC converters or interface circuits. Because PLCs are employed on factory floors that may have motors or other inductive loads and loops, they are susceptible to line transient spikes. Figure 2-1 shows an example of a line voltage transient which may have a short duration, but can severely damage circuits inside PLCs without proper protection.
A protection circuit, or clamping circuit shown in Figure 2-2 would typically be used for protecting the load from voltage spikes. The diode D2 is used to set the clamp voltage and a pass FET is used to allow the current to flow to the load protected. Unfortunately, these circuits take up space and require more additional circuitry. As semiconductor process technology advances, suppliers are able to offer higher input voltage converters to integrate components and save space. It is true that a 28-V converter rated at 3 A is a less expensive than a 60-V, 3-A converter with the same MOSFET resistance. But the reliability and space savings of a higher rated converter is worth the small added price. Instead of relying on voltage protection circuits, non-isolated synchronous buck converters with integrated FETs are available with ratings up to 100 V to protect downstream circuits.
Because PLCs operate in harsh factory environments, they are enclosed in a cabinet where airflow is either constricted or unavailable. In many cases, the use of a cooling fan is prohibited due to the presence of dust, corrosive elements, or other material limitations. Integrated circuits dissipate heat when operating, especially power management devices, so it is important to choose a high efficient power solution to minimize heat. System long-term reliability is degraded under excessive thermal stressing. Heat also affects the accuracy of any analog sensing circuitry. There is a good chance that the amount of power is limited from the 24-V source supplied to the PLC. Reducing the power dissipation of the point-of-load power solution will increase the power budget of a module and allow the PLC to be differentiated in the marketplace. Additional available power allows faster microprocessor clocking speeds, higher accuracy accurate data converters, or additional memory to improve the performance of the PLC against the competition. Harsh factory environments may experience extreme ambient temperature. It is more useful to specify and rate DC/DC converters by their minimum and maximum junction temperature rather than their ambient temperature. Many DC/DC converters are rated at 150C maximum junction temperature to provide more thermal headroom. An operating temperature range parameter is available within the parametric search engine of step down converters which makes it easy to select products with high operating temperature capability.
Operating a DC/DC converter at peak efficiency is an excellent way to minimize the conduction and switching losses of the DC/DC converter’s power MOSFETs. The efficiency of the 2-A TPS54218 design de-rated to 0.5 A is shown in Table 3-1 compared to the 0.5-A TPS62231 using Webench®. Obviously, the smaller MOSFETs of the TPS62231 allow a smaller package size, and the higher frequency allows smaller passive components for smaller solution size. However, the TPS54218 saves 140mW of energy, maximizing efficiency and improving thermal performance in applications that have limited airflow or constrained power budgets. The efficiency of TPS54218 can be further optimized as shown in Figure 3-1. Peak efficiency is about 93% around 0.5A at the knee of the curve which represents the optimal point between switching and conduction losses.
Device | η | Pd (W) | Rds(on) | Frequency | Solution Size |
TPS54218 | 87% | 0.13 | 20 mΩ/20 mΩ | 1.125 MHz | 122 mm2 |
TPS62231 | 80% | 0.27 | 600 mΩ/350 mΩ | 3 MHz | 23 mm2 |