Get started and develop with Bluetooth® low energy (BLE 5.x) solutions
Select a platform
LAUNCHXL-CC1352P1 — CC1352P LaunchPad™ development kit for SimpleLink™ multi-band wireless MCU
LAUNCHXL-CC26X2R1 — CC26x2R SimpleLink™ マルチスタンダード・ワイヤレス・マイコン向け LaunchPad™ 開発キット
LP-CC2652RB — CC2652RB LaunchPad™ development kit for BAW multi-protocol 2.4-GHz SimpleLink™ wireless MCU
LPSTK-CC1352R — SimpleLink™ multi band CC1352R wireless MCU Launchpad™ SensorTag kit
FLASH-PROGRAMMER — SmartRF フラッシュ・プログラマ
FLASH-PROGRAMMER — SmartRF フラッシュ・プログラマ
SIMPLELINK-LOWPOWER-F2-SDK — SimpleLink™ Low Power F2 software development kit (SDK) for the CC13x1, CC13x2, CC13x4, CC26x1, CC26x2 and CC26x4 devices
SIMPLELINK-LOWPOWER-F2-SDK — SimpleLink™ Low Power F2 software development kit (SDK) for the CC13x1, CC13x2, CC13x4, CC26x1, CC26x2 and CC26x4 devices
製品
車載ワイヤレス接続製品
低消費電力 2.4GHz 製品
Sub-1GHz ワイヤレス・マイコン
ハードウェア開発
開発キット
評価ボード
リリース情報
The SimpleLink™ Low Power F2 Software Development Kit (SDK), formerly known as the CC13xx and CC26xx SDK, delivers components that enable engineers to develop applications on the Texas Instruments SimpleLink CC13xx and CC26xx family of wireless microcontrollers (MCUs). This software toolkit provides a cohesive and consistent software experience for all SimpleLink CC13xx and CC26xx wireless MCU users by packaging essential software components, such as a Bluetooth® Low Energy (BLE) protocol stack supporting Bluetooth 5.2, Zigbee 3.0 compliant protocol suite, RF-Proprietary examples, TI’s 15.4 Stack, TI Wi-SUN FAN Stack, Amazon Sidewalk examples, as well as the TI-RTOS7 and FreeRTOS™ kernels and TI Drivers in one easy-to-use software package along with example applications and documentation. In addition, the Dynamic Multi-Protocol Manager (DMM) software component enables multiprotocol development on a single SimpleLink wireless MCU.
Although not included in the SDK, SimpleLink CC13xx and CC26xx wireless MCUs are also capable of supporting the following wireless solutions: Please refer to their respective repositories for resources and more information.
- The Matter standard: https://github.com/TexasInstruments/matter
- Thread 1.1.1 networking stack based on OpenThread: https://github.com/TexasInstruments/ot-ti
The SimpleLink MCU portfolio offers a single development environment that delivers flexible hardware, software, and tool options for customers developing wired and wireless applications. With 100 percent code reuse across host MCUs, Wi-Fi™, Bluetooth Low Energy, Sub-1GHz devices and more, choose the MCU or connectivity standard that fits your design. A one-time investment with the SimpleLink software development kit allows you to reuse often, opening the door to create unlimited applications. For more information, visit www.ti.com/simplelink.
This is version 8.30.01.01 of the SimpleLink Low Power F2 SDK. This version only contains internal metadata updates for integrating with the TI Developer Zone; there are no embedded software changes from the 8.30.00.121 release. This SDK is also available on GitHub at https://github.com/TexasInstruments/simplelink-lowpower-f2-sdk
最新情報
- Example projects and RF settings for the upcoming CC2674P10 LaunchPad™ development kit for SimpleLink multi-standard wireless MCU.
- CCS Theia, now supports all SimpleLink F2 devices. Please use version 1.5.0 or newer. For more information, see Upcoming Features.
- The new TI Log driver simplifies adding log statements to your application without compromising on memory or processing power. The following SW modules are instrumented: Power driver, UART2 driver, TI 15.4-Stack.
- The Wi-SUN gateway example for Linux, wfantund, now supports using external authentication server and/or external DHCP server. It also supports Router Node configuration for the first time.
- The TI Wi-SUN Stack has three new Network Profiles which simplify network configuration.
- MCUboot is updated to version 2.0 and now supports using an encrypted image. You can now configure MCUboot in SysConfig.
- DMM now supports closing a handle, opening the possibility of using more than two handles in one application.
BT-POWER-CALC — Bluetooth Power Calculator for CC13xx, CC26xx and CC23xx devices
BT-POWER-CALC — Bluetooth Power Calculator for CC13xx, CC26xx and CC23xx devices
製品
低消費電力 2.4GHz 製品
Sub-1GHz ワイヤレス・マイコン
車載ワイヤレス接続製品
ハードウェア開発
開発キット
リリース情報
This release adds the Power Estimator for CC23xx devices
最新情報
- CC23xx Power Estimator
SMARTRF-STUDIO-7 — SmartRF スタジオ
SMARTRF-STUDIO-7 — SmartRF スタジオ
製品
MSP430 マイコン
低消費電力 2.4GHz 製品
Sub-1GHz ワイヤレス・マイコン
Sub-1GHz トランシーバ
他のワイヤレス製品
車載ワイヤレス接続製品
ハードウェア開発
開発キット
評価ボード
インターフェイス・アダプタ
ドーター・カード
ドキュメント
SmartRF Studio 7 in Cloud TI Resource Explorer
Compressed source file archive
リリース情報
SmartRF™ Studio is a Windows application that can be used to evaluate and configure Low Power RF devices from Texas Instruments. The application helps designers of RF systems to easily evaluate the radio at an early stage in the design process. It is especially useful for generation of configuration register values and commands, and for practical testing and debugging of the RF system. SmartRF Studio can be used either as a standalone application or together with applicable evaluation boards or debug probes for the RF device.
最新情報
- Updated RF PHY settings for the CC13x4/CC26x4 devices
- Updated target board definitions for LP_EM_CC2674P10
- Various improvements and bug-fixes
CCSTUDIO — Code Composer Studio 統合開発環境(IDE)
CCSTUDIO — Code Composer Studio 統合開発環境(IDE)
こちらの設計リソースは、このカテゴリに属する製品の大半をサポートしています。
サポート状況を確認するには、製品の詳細ページをご覧ください
-
parametric-filter デジタル信号プロセッサ (DSP) -
parametric-filter Arm ベースのプロセッサ -
parametric-filter MSP430 マイコン -
parametric-filter C2000 リアルタイム・マイコン -
parametric-filter Arm ベースのマイコン -
parametric-filter シグナル・コンディショナ -
parametric-filter ミリ波レーダー・センサ -
parametric-filter Wi-Fi 製品 -
parametric-filter Sub-1GHz 製品 -
parametric-filter デジタル電源絶縁型コントローラ
製品
Arm Cortex-M0+ マイコン
Arm Cortex-M4 マイコン
Arm Cortex-R マイコン
車載ミリ波レーダー・センサ
産業用ミリ波レーダー・センサ
Sub-1GHz ワイヤレス・マイコン
ハードウェア開発
評価ボード
開発キット
ドキュメント
リリース情報
The Code Composer Studio™ IDE is a complete integrated suite that enables developers to create and debug applications of all Texas Instruments Embedded Processors (Sitara, DSP, Automotive, Keystone), Microcontrollers (SimpleLink™, C2000 Digital Control, MSP430, TM4C, Hercules), as well as Digital Power (UCD) and Programmable Gain Amplifier (PGA) devices.
CCS v20 is TI’s next generation Integrated Development Environment (IDE) based on Theia IDE framework. CCS v20.1.0 uses a modified version of the Theia-IDE framework and offers a user experience similar to Visual Studio Code™.
- Installation instructions and User's Guide
- Windows 32bit is not supported with CCSv20.
- XDS510 class debug probes are not supported with CCSv20.
最新情報
- IDE features improvements (Projects, Memory View, Watch View, Breakpoints, etc.)
- Startup improvement on macOS version with Arm® processors
- Note: the Theia IDE component is now compiled for Arm® processors for performance improvements, but the backend components are still x86 based, so Rosetta is still required.
- Device Support Updates (added AM62L support, added xWRL68xx support, added MSPM0C110x support, various improvements to LPCS flash library, various improvements and bug fixes for F28 and F29 devices)
- Compiler Updates (TI ARM Clang v4.0.2. More info: https://www.ti.com/tool/download/ARM-CGT-CLANG)
- SysConfig v1.23 supporting the latest devices, features improvements, bug fixes (more info: https://www.ti.com/tool/download/SYSCONFIG)
- Updated to latest J-Link support package (v8.12.4)
- Various enhancements and bug fixes
UNIFLASH — ほとんどの TI 製マイコン(MCU)とミリ波センサに対応する UniFlash
UNIFLASH — ほとんどの TI 製マイコン(MCU)とミリ波センサに対応する UniFlash
製品
C2000 リアルタイム・マイコン
Arm ベースのプロセッサ
Arm Cortex-M0+ マイコン
Arm Cortex-R マイコン
車載ミリ波レーダー・センサ
産業用ミリ波レーダー・センサ
リリース情報
UniFlash is a standalone tool used to program on-chip and external flash memory on TI MCUs and on-board flash memory for Sitara processors. UniFlash has a GUI, command line, and scripting interface. UniFlash is available free of charge.
最新情報
- Device support sync-up with CCS v20.1.0
- Updated J-Link support package (v8.12.4)
- Updated Image Creator package (v3.24.4.1)
- Updated MSP Bootloader package for macOS (v1.7.0.0)
- Added ability to split the program and verify steps in a generated CLI package, to improve the flow for some security devices
- For Connectivity devices, added a setting to control if UniFlash will switch to a different configuration during connect for locked boards
- various bug fixes
SENSOR-CONTROLLER-STUDIO — センサ・コントローラ・スタジオ
SENSOR-CONTROLLER-STUDIO — センサ・コントローラ・スタジオ
Installer executable
Compressed archive
製品
低消費電力 2.4GHz 製品
Sub-1GHz ワイヤレス・マイコン
他のワイヤレス製品
車載ワイヤレス接続製品
ハードウェア開発
開発キット
評価ボード
ドキュメント
Compressed source file archive
リリース情報
Sensor Controller Studio is used to write, test and debug code for the CC26xx/CC13xx Sensor Controller, allowing for ultra-low power application design.
The tool generates a Sensor Controller Interface driver, which is a set of C source files to be compiled into the System CPU (ARM Cortex-M3/M4) application. These source files contain the Sensor Controller firmware image and associated definitions, and generic functions that allow the System CPU application to control the Sensor Controller and exchange data.
The Sensor Controller is a small CPU core that is highly optimized for low power consumption and efficient peripheral operation. The Sensor Controller is located in the CC26xx/CC13xx auxiliary (AUX) power/clock domain, and can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power state. Such tasks include but are not limited to:
- Analog sensor polling, using ADC or comparator
- Digital sensor polling, using SPI, I2C or other protocols
- Capacitive sensing, using current source, comparator and time-to-digital converter (TDC)
- Waveform generation, for example for LCDs
The Sensor Controller is user programmable, using a simple programming language with syntax similar to C. This allows for sensor polling and other tasks to be specified as sequential algorithms, rather than static configuration of complex peripheral modules, timers, DMA, register programmable state machines, event routing and so on. The main advantages are:
- Flexibility
- Dynamic reuse of hardware resources
- Ability to perform simple data processing without need for dedicated hardware
- Observability and debugging options
最新情報
- Added support for new devices: CC2672R3, CC2672P3, CC2662R-Q1, CC2652PSIP and CC2652P7.
- Added example support for new SDKs, using TI-RTOS 7 and GPIO driver for the latest CC13x2/CC26x2 SDK.
- Minor improvements.
- Bug-fixes.
SIMPLELINK-LOWPOWER-F2-SDK — SimpleLink™ Low Power F2 software development kit (SDK) for the CC13x1, CC13x2, CC13x4, CC26x1, CC26x2 and CC26x4 devices
SIMPLELINK-LOWPOWER-F2-SDK — SimpleLink™ Low Power F2 software development kit (SDK) for the CC13x1, CC13x2, CC13x4, CC26x1, CC26x2 and CC26x4 devices
製品
車載ワイヤレス接続製品
低消費電力 2.4GHz 製品
Sub-1GHz ワイヤレス・マイコン
ハードウェア開発
開発キット
評価ボード
リリース情報
The SimpleLink™ Low Power F2 Software Development Kit (SDK), formerly known as the CC13xx and CC26xx SDK, delivers components that enable engineers to develop applications on the Texas Instruments SimpleLink CC13xx and CC26xx family of wireless microcontrollers (MCUs). This software toolkit provides a cohesive and consistent software experience for all SimpleLink CC13xx and CC26xx wireless MCU users by packaging essential software components, such as a Bluetooth® Low Energy (BLE) protocol stack supporting Bluetooth 5.2, Zigbee 3.0 compliant protocol suite, RF-Proprietary examples, TI’s 15.4 Stack, TI Wi-SUN FAN Stack, Amazon Sidewalk examples, as well as the TI-RTOS7 and FreeRTOS™ kernels and TI Drivers in one easy-to-use software package along with example applications and documentation. In addition, the Dynamic Multi-Protocol Manager (DMM) software component enables multiprotocol development on a single SimpleLink wireless MCU.
Although not included in the SDK, SimpleLink CC13xx and CC26xx wireless MCUs are also capable of supporting the following wireless solutions: Please refer to their respective repositories for resources and more information.
- The Matter standard: https://github.com/TexasInstruments/matter
- Thread 1.1.1 networking stack based on OpenThread: https://github.com/TexasInstruments/ot-ti
The SimpleLink MCU portfolio offers a single development environment that delivers flexible hardware, software, and tool options for customers developing wired and wireless applications. With 100 percent code reuse across host MCUs, Wi-Fi™, Bluetooth Low Energy, Sub-1GHz devices and more, choose the MCU or connectivity standard that fits your design. A one-time investment with the SimpleLink software development kit allows you to reuse often, opening the door to create unlimited applications. For more information, visit www.ti.com/simplelink.
This is version 8.30.01.01 of the SimpleLink Low Power F2 SDK. This version only contains internal metadata updates for integrating with the TI Developer Zone; there are no embedded software changes from the 8.30.00.121 release. This SDK is also available on GitHub at https://github.com/TexasInstruments/simplelink-lowpower-f2-sdk
最新情報
- Example projects and RF settings for the upcoming CC2674P10 LaunchPad™ development kit for SimpleLink multi-standard wireless MCU.
- CCS Theia, now supports all SimpleLink F2 devices. Please use version 1.5.0 or newer. For more information, see Upcoming Features.
- The new TI Log driver simplifies adding log statements to your application without compromising on memory or processing power. The following SW modules are instrumented: Power driver, UART2 driver, TI 15.4-Stack.
- The Wi-SUN gateway example for Linux, wfantund, now supports using external authentication server and/or external DHCP server. It also supports Router Node configuration for the first time.
- The TI Wi-SUN Stack has three new Network Profiles which simplify network configuration.
- MCUboot is updated to version 2.0 and now supports using an encrypted image. You can now configure MCUboot in SysConfig.
- DMM now supports closing a handle, opening the possibility of using more than two handles in one application.
SENSOR-CONTROLLER-STUDIO — センサ・コントローラ・スタジオ
SENSOR-CONTROLLER-STUDIO — センサ・コントローラ・スタジオ
Installer executable
Compressed archive
製品
低消費電力 2.4GHz 製品
Sub-1GHz ワイヤレス・マイコン
他のワイヤレス製品
車載ワイヤレス接続製品
ハードウェア開発
開発キット
評価ボード
ドキュメント
Compressed source file archive
リリース情報
Sensor Controller Studio is used to write, test and debug code for the CC26xx/CC13xx Sensor Controller, allowing for ultra-low power application design.
The tool generates a Sensor Controller Interface driver, which is a set of C source files to be compiled into the System CPU (ARM Cortex-M3/M4) application. These source files contain the Sensor Controller firmware image and associated definitions, and generic functions that allow the System CPU application to control the Sensor Controller and exchange data.
The Sensor Controller is a small CPU core that is highly optimized for low power consumption and efficient peripheral operation. The Sensor Controller is located in the CC26xx/CC13xx auxiliary (AUX) power/clock domain, and can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power state. Such tasks include but are not limited to:
- Analog sensor polling, using ADC or comparator
- Digital sensor polling, using SPI, I2C or other protocols
- Capacitive sensing, using current source, comparator and time-to-digital converter (TDC)
- Waveform generation, for example for LCDs
The Sensor Controller is user programmable, using a simple programming language with syntax similar to C. This allows for sensor polling and other tasks to be specified as sequential algorithms, rather than static configuration of complex peripheral modules, timers, DMA, register programmable state machines, event routing and so on. The main advantages are:
- Flexibility
- Dynamic reuse of hardware resources
- Ability to perform simple data processing without need for dedicated hardware
- Observability and debugging options
最新情報
- Added support for new devices: CC2672R3, CC2672P3, CC2662R-Q1, CC2652PSIP and CC2652P7.
- Added example support for new SDKs, using TI-RTOS 7 and GPIO driver for the latest CC13x2/CC26x2 SDK.
- Minor improvements.
- Bug-fixes.
PACKET-SNIFFER — SmartRF™ Packet Sniffer 2.18.1
PACKET-SNIFFER — SmartRF™ Packet Sniffer 2.18.1
製品
低消費電力 2.4GHz 製品
Sub-1GHz ワイヤレス・マイコン
Sub-1GHz トランシーバ
他のワイヤレス製品
車載ワイヤレス接続製品
ハードウェア開発
評価ボード
開発キット
リリース情報
UNIFLASH — ほとんどの TI 製マイコン(MCU)とミリ波センサに対応する UniFlash
UNIFLASH — ほとんどの TI 製マイコン(MCU)とミリ波センサに対応する UniFlash
製品
C2000 リアルタイム・マイコン
Arm ベースのプロセッサ
Arm Cortex-M0+ マイコン
Arm Cortex-R マイコン
車載ミリ波レーダー・センサ
産業用ミリ波レーダー・センサ
リリース情報
UniFlash is a standalone tool used to program on-chip and external flash memory on TI MCUs and on-board flash memory for Sitara processors. UniFlash has a GUI, command line, and scripting interface. UniFlash is available free of charge.
最新情報
- Device support sync-up with CCS v20.1.0
- Updated J-Link support package (v8.12.4)
- Updated Image Creator package (v3.24.4.1)
- Updated MSP Bootloader package for macOS (v1.7.0.0)
- Added ability to split the program and verify steps in a generated CLI package, to improve the flow for some security devices
- For Connectivity devices, added a setting to control if UniFlash will switch to a different configuration during connect for locked boards
- various bug fixes
BT-POWER-CALC — Bluetooth Power Calculator for CC13xx, CC26xx and CC23xx devices
BT-POWER-CALC — Bluetooth Power Calculator for CC13xx, CC26xx and CC23xx devices
製品
低消費電力 2.4GHz 製品
Sub-1GHz ワイヤレス・マイコン
車載ワイヤレス接続製品
ハードウェア開発
開発キット
リリース情報
This release adds the Power Estimator for CC23xx devices
最新情報
- CC23xx Power Estimator
SMARTRF-STUDIO-7 — SmartRF スタジオ
SMARTRF-STUDIO-7 — SmartRF スタジオ
製品
MSP430 マイコン
低消費電力 2.4GHz 製品
Sub-1GHz ワイヤレス・マイコン
Sub-1GHz トランシーバ
他のワイヤレス製品
車載ワイヤレス接続製品
ハードウェア開発
開発キット
評価ボード
インターフェイス・アダプタ
ドーター・カード
ドキュメント
SmartRF Studio 7 in Cloud TI Resource Explorer
Compressed source file archive
リリース情報
SmartRF™ Studio is a Windows application that can be used to evaluate and configure Low Power RF devices from Texas Instruments. The application helps designers of RF systems to easily evaluate the radio at an early stage in the design process. It is especially useful for generation of configuration register values and commands, and for practical testing and debugging of the RF system. SmartRF Studio can be used either as a standalone application or together with applicable evaluation boards or debug probes for the RF device.
最新情報
- Updated RF PHY settings for the CC13x4/CC26x4 devices
- Updated target board definitions for LP_EM_CC2674P10
- Various improvements and bug-fixes